TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
snpConnEstEvt_t Struct Reference

Parameter Structure for the Connection Established Event. More...

Data Fields

uint8_t addressType
 1 Byte Type of initiator address
 
uint16_t connHandle
 2 Byte Handle of the connection
 
uint16_t connInterval
 2 Byte More...
 
uint8_t pAddr [6]
 6 Byte Address of the initiator
 
uint16_t slaveLatency
 2 Byte More...
 
uint16_t supervisionTimeout
 2 Byte More...
 

Detailed Description

Parameter Structure for the Connection Established Event.

See SNP Event Indication for more information.

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.

Field Documentation

§ connInterval

uint16_t connInterval

2 Byte

See also
snpUpdateConnParamReq_t::connInterval

§ slaveLatency

uint16_t slaveLatency

§ supervisionTimeout

uint16_t supervisionTimeout

The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated