TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
snpAddAttrFormat_t Struct Reference

Parameter Structure used to add a Format attribute. More...

Data Fields

uint16_t desc
 < 1 Byte Namespace, as described by BLE Spec, Vol 3, Part G, Chapter 3.3 More...
 
uint8_t exponent
 1 Byte Exponent, as described by BLE Spec, Vol 3, Part G, Chapter 3.3
 
uint8_t format
 1 Byte Format, as described by BLE Spec, Vol 3, Part G, Chapter 3.3
 
uint16_t unit
 2 Byte Unit, as described by BLE Spec, Vol 3, Part G, Chapter 3.3
 

Detailed Description

Parameter Structure used to add a Format attribute.

Used with snpAddCharDescDeclReq_t

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.

Field Documentation

§ desc

uint16_t desc

< 1 Byte Namespace, as described by BLE Spec, Vol 3, Part G, Chapter 3.3

2 Byte Desc, as described by BLE Spec, Vol 3, Part G, Chapter 3.3


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated