TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
snpConnTermEvt_t Struct Reference

Parameter Structure for the Connection terminated Event. More...

Data Fields

uint16_t connHandle
 2 Byte Handle of the connection
 
uint8_t reason
 1 Byte Reason of the termination connection termination reason.
 

Detailed Description

Parameter Structure for the Connection terminated Event.

See SNP Event Indication for more information.

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated