TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
snpSetAttrValueRsp_t Struct Reference

Parameter Structure for response to SNP_setAttrValue / SNP_SET_ATTR_VALUE_RSP. More...

Data Fields

uint16_t attrHandle
 2 Byte Attribute handle of the characteristic value.
 
uint8_t status
 1 Byte Status of the request (SUCCESS or Error, list of status generated by the SNP.)
 

Detailed Description

Parameter Structure for response to SNP_setAttrValue / SNP_SET_ATTR_VALUE_RSP.

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated