TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
snpGetRevisionRsp_t Struct Reference

Parameter Structure for SNP_getRev. More...

Data Fields

uint16_t snpVer
 2 Byte Version of the SNP (major, minor)
 
uint8_t stackBuildVer [10]
 10 Byte Stack Revision see TI HCI vendor guide.
 
uint8_t status
 1 Byte status of the request (SUCCESS or Error, list of status generated by the SNP.)
 

Detailed Description

Parameter Structure for SNP_getRev.

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated