TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
snpSetGattParamReq_t Struct Reference

Parameter Structure for SNP_setGATTParam / SNP_SET_GATT_PARAM_RSP. More...

Data Fields

uint8_t paramID
 1 Byte ID of the parameter of the service to update/retrieved
 
uint8_t * pData
 Pointer of Data to write/retrieved.
 
uint8_t serviceID
 

Detailed Description

Parameter Structure for SNP_setGATTParam / SNP_SET_GATT_PARAM_RSP.

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.

Field Documentation

§ serviceID

uint8_t serviceID

1 Byte ID of the service containing the parameter

Existing list of service can be found here: see Predefined services


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated