TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
snpTestCmdRsp_t Struct Reference

Parameter Structure for SNP_executeTestCmd. More...

Data Fields

uint16_t memAlo
 2 Byte HEAP allocated memory
 
uint16_t memMax
 2 Byte maximum HEAP ever allocated since startup
 
uint16_t memSize
 2 Byte total HEAP size
 

Detailed Description

Parameter Structure for SNP_executeTestCmd.

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated