TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
snpAddAttrCccd_t Struct Reference

Parameter Structure used to add a Client Characteristic Configuration Description Attribute. More...

Data Fields

uint8_t perms
 1 Byte permissions of the attribute, GATT Attribute Access Permissions Bit Fields
 

Detailed Description

Parameter Structure used to add a Client Characteristic Configuration Description Attribute.

Used with snpAddCharDescDeclReq_t

snpAddAttrCccd_t::perms are defined by a profile or are implementation specific. TI BLE-Stack has define its own permissions: GATT Attribute Access Permissions Bit Fields.
Basic filtering is done using those values For example, a read request on a characteristic value which does not permit reading will be rejected by the stack without AP interaction.
This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated