TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
snpSetGattParamRsp_t Struct Reference

1 Byte Command Status Response More...

Data Fields

uint8_t status
 1 Byte Command Status (SUCCESS or Error, list of status generated by the SNP.)
 

Detailed Description

1 Byte Command Status Response

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated