TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
snpErrorEvt_t Struct Reference

Parameter Structure for the Error Event SNP_ERROR_EVT. More...

Data Fields

uint16_t opcode
 2 Byte SNP opcode that triggered the error
 
uint8_t status
 1 Byte Status of the request list of status generated by the SNP.
 

Detailed Description

Parameter Structure for the Error Event SNP_ERROR_EVT.

See SNP Event Indication for more information.

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated