2.5. Linux Setup

This guide provides Linux-specific instructions for installing Tiny ML Tensorlab. Linux is the primary development platform for the toolchain.

2.5.1. System Preparation

Ubuntu/Debian

# Update system
sudo apt update && sudo apt upgrade -y

# Install essential packages
sudo apt install -y build-essential git curl wget \
    libssl-dev zlib1g-dev libbz2-dev libreadline-dev \
    libsqlite3-dev libncursesw5-dev xz-utils tk-dev \
    libxml2-dev libxmlsec1-dev libffi-dev liblzma-dev

Fedora/RHEL

sudo dnf install -y git curl wget make gcc gcc-c++ \
    openssl-devel bzip2-devel libffi-devel zlib-devel \
    readline-devel sqlite-devel ncurses-devel xz-devel

2.5.2. Installing Python 3.10

We recommend using pyenv for Python version management:

# Install pyenv
curl https://pyenv.run | bash

# Add to ~/.bashrc (or ~/.zshrc for zsh users)
echo 'export PYENV_ROOT="$HOME/.pyenv"' >> ~/.bashrc
echo 'export PATH="$PYENV_ROOT/bin:$PATH"' >> ~/.bashrc
echo 'eval "$(pyenv init -)"' >> ~/.bashrc

# Reload shell
source ~/.bashrc

# Install Python 3.10
pyenv install 3.10.14

# Set as global default
pyenv global 3.10.14

# Verify
python --version  # Should show Python 3.10.14

2.5.3. Installation

Option A: Automated Setup (Recommended)

# Clone repository
git clone https://github.com/TexasInstruments/tinyml-tensorlab.git
cd tinyml-tensorlab/tinyml-modelmaker

# Run setup script
./setup_all.sh

The script handles:

  • Virtual environment creation

  • Dependency installation

  • Editable installation of all components

Option B: Manual Installation

# Clone repository
git clone https://github.com/TexasInstruments/tinyml-tensorlab.git
cd tinyml-tensorlab

# Create virtual environment
python -m venv venv
source venv/bin/activate

# Upgrade pip and build tools
pip install --upgrade pip setuptools wheel

# Install components
pip install -e tinyml-modelmaker
pip install -e tinyml-tinyverse
pip install -e tinyml-modeloptimization/torchmodelopt
pip install -e tinyml-modelzoo

2.5.4. Verification

# Activate environment
source venv/bin/activate

# Verify Python packages
python -c "import tinyml_modelmaker; print('OK')"
python -c "import tinyml_tinyverse; print('OK')"
python -c "import tinyml_modelzoo; print('OK')"
python -c "import tinyml_torchmodelopt; print('OK')"

Configure Environment Variables

Warning

IMPORTANT: Environment Variables Required for Model Compilation

For AI model compilation to work, you MUST set environment variables specific to your target device before running examples.

The variables you need depend on which device you’re targeting:

  • C2000 devices (F28P55, F28P65, etc.): Set C2000_CG_ROOT and C2000WARE_ROOT

  • F29 devices (F29H85X, etc.): Set CG_TOOL_ROOT

  • MSPM0 devices: Set ARM_LLVM_CGT_PATH

  • AM13E devices: Set ARM_LLVM_CGT_PATH

  • AM26x devices: Set ARM_LLVM_CGT_PATH

  • Connectivity devices (CC2755, CC1352, etc.): Set ARM_LLVM_CGT_PATH

See Environment Variables for complete device-specific setup instructions.

Run Hello World Example

# Activate environment
source venv/bin/activate

# Run hello world example
cd tinyml-modelzoo
./run_tinyml_modelzoo.sh examples/generic_timeseries_classification/config.yaml

2.5.5. Speeding Up Installation

The installation process can take 15-30 minutes due to downloading large packages. Here are ways to make it faster:

Use setup_all.sh (Parallel Installation)

This is the fastest method:

cd tinyml-tensorlab/tinyml-modelmaker
./setup_all.sh

This typically completes in 10-15 minutes (vs 20-30 minutes for manual installation).

Enable pip Caching for Future Installs

# Create pip config
mkdir -p ~/.pip
cat > ~/.pip/pip.conf << EOF
[global]
cache-dir = ~/.cache/pip
no-cache-dir = False
EOF

Subsequent reinstalls will use cached packages and complete in 5-10 minutes.

Use CPU-Only PyTorch (If No GPU)

If you don’t need GPU support:

pip install torch torchvision --index-url https://download.pytorch.org/whl/cpu
pip install -e tinyml-modelmaker
# ... rest of installation

This skips CUDA components and saves 5-10 minutes.

Check Installation Progress

To monitor downloads in real-time:

pip install --verbose -e tinyml-modelmaker

2.5.6. GPU Setup (Optional)

For NVIDIA GPU support (useful for NAS):

Install NVIDIA Drivers

# Ubuntu
sudo apt install -y nvidia-driver-535  # Or latest version

# Verify
nvidia-smi

Install CUDA Toolkit

Download from https://developer.nvidia.com/cuda-downloads

Or use conda/pip:

# PyTorch with CUDA is installed automatically
# Verify CUDA availability
python -c "import torch; print(f'CUDA available: {torch.cuda.is_available()}')"

2.5.7. Shell Configuration

Alias for Quick Access

Add to ~/.bashrc:

# Tiny ML Tensorlab aliases
alias tensorlab='cd ~/tinyml-tensorlab && source venv/bin/activate'
alias run-tensorlab='./run_tinyml_modelzoo.sh'

Auto-activate Environment

For automatic activation when entering the directory:

# Add to ~/.bashrc
function cd() {
    builtin cd "$@"
    if [ -f "venv/bin/activate" ]; then
        source venv/bin/activate
    fi
}

2.5.8. Permission Issues

Make Scripts Executable

chmod +x tinyml-modelzoo/run_tinyml_modelzoo.sh
chmod +x tinyml-modelmaker/run_tinyml_modelmaker.sh
chmod +x tinyml-modelmaker/setup_all.sh

Fix Permission Denied Errors

If you encounter permission errors:

# Check file ownership
ls -la

# Fix ownership if needed
sudo chown -R $USER:$USER ~/tinyml-tensorlab

2.5.9. Multiple Python Versions

If you need to manage multiple Python projects:

# Set local version for this project only
cd ~/tinyml-tensorlab
pyenv local 3.10.14

# This creates a .python-version file
# Python 3.10 will be used automatically in this directory

2.5.10. System Service (Optional)

For running training jobs as a background service:

Create /etc/systemd/system/tensorlab-training.service:

[Unit]
Description=Tiny ML Training Job
After=network.target

[Service]
Type=simple
User=your_username
WorkingDirectory=/home/your_username/tinyml-tensorlab/tinyml-modelzoo
ExecStart=/home/your_username/tinyml-tensorlab/venv/bin/python -m tinyml_modelmaker config.yaml
Restart=no

[Install]
WantedBy=multi-user.target

2.5.11. Troubleshooting

“pyenv: command not found”

Ensure pyenv is in your PATH:

source ~/.bashrc
# Or log out and log back in

CUDA out of memory

Reduce batch size or use CPU:

training:
  batch_size: 64  # Reduce from 256
  num_gpus: 0     # Use CPU

Slow training without GPU

This is expected. For faster training:

  • Use a smaller model

  • Reduce training epochs

  • Use Google Colab with free GPU

2.5.12. Next Steps