2.3. Developer Installation
This guide covers the full installation method for developers who want to customize models, add features, or contribute to Tiny ML Tensorlab.
2.3.1. Overview
Developer installation involves:
Cloning the repository
Creating a Python virtual environment
Installing all components in editable mode
Configuring environment variables
2.3.2. Step 1: Clone the Repository
git clone https://github.com/TexasInstruments/tinyml-tensorlab.git
cd tinyml-tensorlab
2.3.3. Step 2: Set Up Python Environment
Option A: Using setup_all.sh (Linux - Recommended)
The easiest method on Linux:
cd tinyml-modelmaker
./setup_all.sh
This script:
Creates a virtual environment using pyenv
Installs all dependencies
Installs all components in editable mode
Option B: Manual Installation
If the script doesn’t work or you’re on Windows:
# Create virtual environment
python -m venv venv
source venv/bin/activate
# Upgrade pip and build tools
pip install --upgrade pip setuptools wheel
# Install components in order
pip install -e tinyml-modelmaker
pip install -e tinyml-tinyverse
pip install -e tinyml-modeloptimization/torchmodelopt
pip install -e tinyml-modelzoo
# Create virtual environment
python -m venv venv
.\venv\Scripts\Activate.ps1
# Upgrade pip and build tools
python -m pip install --upgrade pip setuptools wheel
# Install components in order
pip install -e tinyml-modelmaker
pip install -e tinyml-tinyverse
pip install -e tinyml-modeloptimization\torchmodelopt
pip install -e tinyml-modelzoo
2.3.4. Step 3: Verify Installation
Verify all components are installed by importing the packages and checking versions:
import tinyml_modelmaker
import tinyml_tinyverse
import tinyml_torchmodelopt
import tinyml_modelzoo
print(f"TI Tiny ML ModelMaker: {tinyml_modelmaker.__version__}")
print(f"TI Tiny ML Tinyverse: {tinyml_tinyverse.__version__}")
print(f"TI Tiny ML Model Optimization toolkit: {tinyml_torchmodelopt.__version__}")
print(f"TI Tiny ML Model Zoo: {tinyml_modelzoo.__version__}")
If all packages import without errors and versions are displayed, your installation is complete.
2.3.5. Step 4: Configure Environment Variables
Warning
IMPORTANT: Environment Variables Required for Model Compilation
For AI model compilation to work, you MUST set environment variables specific to your target device before running examples.
The variables you need depend on which device you’re targeting:
C2000 devices (F28P55, F28P65, etc.): Set
C2000_CG_ROOTandC2000WARE_ROOTF29 devices (F29H85X, etc.): Set
CG_TOOL_ROOTMSPM0 devices: Set
ARM_LLVM_CGT_PATHAM13E devices: Set
ARM_LLVM_CGT_PATHAM26x devices: Set
ARM_LLVM_CGT_PATHConnectivity devices (CC2755, CC1352, etc.): Set
ARM_LLVM_CGT_PATH
See Environment Variables for complete device-specific setup instructions.
Step 5: Run the hello world example:
cd tinyml-modelzoo
./run_tinyml_modelzoo.sh examples/generic_timeseries_classification/config.yaml
cd tinyml-modelzoo
run_tinyml_modelzoo.bat examples\generic_timeseries_classification\config.yaml
2.3.6. Directory Structure After Installation
tinyml-tensorlab/
├── tinyml-modelmaker/
│ ├── tinyml_modelmaker/ # Source code (editable)
│ ├── examples/
│ ├── docs/
│ └── data/ # Created on first run
│ └── projects/ # Training outputs
├── tinyml-tinyverse/
│ └── tinyml_tinyverse/ # Source code (editable)
├── tinyml-modeloptimization/
│ └── torchmodelopt/
│ └── tinyml_torchmodelopt/ # Source code (editable)
├── tinyml-modelzoo/
│ ├── tinyml_modelzoo/ # Source code (editable)
│ └── examples/ # Entry point configs
└── venv/ # Virtual environment
2.3.7. Updating
Using git_pull_all.sh (Recommended)
The simplest way to keep all repositories up to date:
./git_pull_all.sh
This script pulls the latest changes for all sub-repositories in one step.
Manual Update
Alternatively, update each component manually:
# Update from GitHub
git pull origin main
# Reinstall components if dependencies changed
pip install -e tinyml-modelmaker
pip install -e tinyml-tinyverse
pip install -e tinyml-modeloptimization/torchmodelopt
pip install -e tinyml-modelzoo
2.3.8. Common Developer Tasks
Adding a New Model
Edit files in tinyml-modelzoo/tinyml_modelzoo/models/:
# tinyml_modelzoo/models/classification.py
class MY_NEW_MODEL(GenericModelWithSpec):
...
Modifying Training Scripts
Edit files in tinyml-tinyverse/tinyml_tinyverse/references/:
# Example: classification training
vim tinyml-tinyverse/tinyml_tinyverse/references/timeseries_classification/train.py
Adding Custom Transforms
Edit files in tinyml-tinyverse/tinyml_tinyverse/common/transforms/.
2.3.9. Speeding Up Installation
The developer installation can take significant time due to downloading large dependencies (PyTorch, TensorFlow, etc.). Here are several ways to speed it up:
Option 1: Use setup_all.sh with Parallel Installation (Linux)
The setup_all.sh script automatically uses parallel builds:
cd tinyml-modelmaker
./setup_all.sh
This is typically 2-3x faster than manual installation.
Option 2: Enable pip Caching
Create or update ~/.pip/pip.conf to enable aggressive caching:
[global]
cache-dir = ~/.cache/pip
no-cache-dir = False
This caches downloaded packages so reinstalls are faster.
Option 3: Use Pre-built Wheels
Ensure pip uses pre-built wheels instead of compiling from source:
pip install --upgrade pip setuptools wheel
pip install -e tinyml-modelmaker # Will use wheels if available
Option 4: Skip Optional GPU Dependencies (If Not Needed)
If you don’t need GPU support, you can use CPU-only PyTorch:
# CPU-only PyTorch (faster to install)
pip install torch==2.0.0 torchvision==0.15.1 --index-url https://download.pytorch.org/whl/cpu
# Then install components
pip install -e tinyml-modelmaker
pip install -e tinyml-tinyverse
pip install -e tinyml-modeloptimization/torchmodelopt
pip install -e tinyml-modelzoo
Option 5: Use Faster Package Index
Some regions may have mirror repositories. For example, in China:
pip install -i https://pypi.tsinghua.edu.cn/simple -e tinyml-modelmaker
Note
Installation Times (Approximate)
Full developer install (first time): 15-30 minutes
With caching enabled (subsequent installs): 5-10 minutes
Using setup_all.sh (Linux): 10-15 minutes
Tip
Checking Download Progress
To see real-time download progress:
pip install --verbose -e tinyml-modelmaker
2.3.10. Troubleshooting
“ModuleNotFoundError” after installation
Ensure you’re in the correct virtual environment:
which python # Should point to your venv
source venv/bin/activate # Reactivate if needed
Dependency conflicts
Try reinstalling in a fresh environment:
rm -rf venv
python -m venv venv
source venv/bin/activate
# Reinstall all components
Permission errors on Linux
Make scripts executable:
chmod +x tinyml-modelzoo/run_tinyml_modelzoo.sh
chmod +x tinyml-modelmaker/run_tinyml_modelmaker.sh
2.3.11. Next Steps
Environment Variables - Configure compilation tools
Quickstart - Train your first model
Adding Custom Models - Add custom models