9.2. NPU Device Deployment

This guide covers deployment to TI devices with Neural Processing Unit (NPU) hardware acceleration.

9.2.1. NPU-Enabled Devices

The following devices include TI’s TINPU:

Device

Family

NPU Features

F28P55

C2000

8-bit/4-bit inference, up to 60k params

AM13E2

AM13

8-bit inference, Cortex-M33 + NPU

MSPM0G5187

MSPM0

8-bit inference, ultra-low power

9.2.2. NPU Compilation

To compile for NPU, use the correct preset:

common:
  target_device: 'F28P55'  # NPU device

training:
  model_name: 'CLS_4k_NPU'  # NPU-compatible model

compilation:
  enable: True
  preset_name: 'compress_npu_layer_data'  # NPU optimization

The compress_npu_layer_data preset:

  • Optimizes memory layout for NPU

  • Compresses weight data

  • Generates NPU-specific code

9.2.3. NPU Model Requirements

Models must follow NPU constraints (see NPU Guidelines):

  • Use model names ending in _NPU

  • Channel counts must be multiples of 4

  • Kernel heights ≤ 7

  • Must use INT8 or INT4 quantization

9.2.4. NPU Compilation Artifacts

After compilation:

.../compilation/artifacts/
├── mod.a                       # Compiled library (includes NPU code)
├── mod.h                       # Model interface
├── model_config.h              # NPU configuration
├── npu_layer_data.bin          # NPU weight data
├── feature_extraction.c        # Feature extraction
└── inference_example.c         # Example code

9.2.5. NPU Initialization

NPU requires initialization before inference:

#include "mod.h"
#include "npu.h"

void main(void) {
    // Initialize system
    System_Init();

    // Initialize NPU hardware
    NPU_Init();

    // Initialize model (loads weights to NPU)
    mod_init();

    // Now ready for inference
    while (1) {
        if (data_ready) {
            run_npu_inference();
        }
    }
}

9.2.6. NPU Inference Code

#include "mod.h"
#include "feature_extraction.h"

// Buffers
float input_buffer[INPUT_SIZE];
float feature_buffer[FEATURE_SIZE];
float output_buffer[NUM_CLASSES];

void run_npu_inference(void) {
    // 1. Collect sensor data
    collect_sensor_data(input_buffer);

    // 2. Extract features (runs on CPU)
    extract_features(input_buffer, feature_buffer);

    // 3. Run NPU inference
    // NPU handles quantization internally
    mod_inference(feature_buffer, output_buffer);

    // 4. Get prediction
    int prediction = argmax(output_buffer, NUM_CLASSES);

    // 5. Act on result
    handle_prediction(prediction);
}

9.2.7. NPU Memory Management

NPU requires specific memory regions:

Weight Memory:

NPU weights are stored in dedicated memory:

// Linker command file
MEMORY
{
    NPU_WEIGHTS : origin = 0x00080000, length = 0x00010000
}

SECTIONS
{
    .npu_weights : > NPU_WEIGHTS
}

Activation Memory:

NPU uses scratch memory for intermediate results:

// Allocate NPU scratch buffer
#pragma DATA_SECTION(npu_scratch, ".npu_scratch")
uint8_t npu_scratch[NPU_SCRATCH_SIZE];

9.2.8. NPU Performance

Typical NPU performance on F28P55:

Model

CPU Time

NPU Time

Speedup

CLS_1k_NPU

2000 µs

150 µs

13x

CLS_4k_NPU

5000 µs

300 µs

17x

CLS_13k_NPU

15000 µs

600 µs

25x

Note: Actual performance depends on model architecture and input size.

9.2.9. NPU Power Considerations

NPU can be power-managed:

// Disable NPU when not in use
void enter_low_power(void) {
    NPU_Disable();  // Saves power
}

// Re-enable before inference
void prepare_inference(void) {
    NPU_Enable();
    // May need small delay for NPU to stabilize
    delay_us(10);
}

9.2.10. NPU Debugging

Verify NPU Initialization:

if (NPU_GetStatus() != NPU_STATUS_READY) {
    // NPU initialization failed
    handle_error();
}

Check Inference Results:

Compare NPU results with expected values from training:

// Known test input
float test_input[] = {...};
float expected_output[] = {...};

mod_inference(test_input, output_buffer);

// Compare
float max_error = 0;
for (int i = 0; i < NUM_CLASSES; i++) {
    float error = fabs(output_buffer[i] - expected_output[i]);
    if (error > max_error) max_error = error;
}

// Quantization error should be small
if (max_error > 0.1) {
    // Unexpected deviation
    debug_print("Max error: %f\n", max_error);
}

9.2.11. NPU Error Handling

Handle NPU errors gracefully:

int run_safe_inference(float* features, float* output) {
    // Check NPU status
    if (NPU_GetStatus() != NPU_STATUS_READY) {
        NPU_Reset();
        if (NPU_GetStatus() != NPU_STATUS_READY) {
            return -1;  // NPU unavailable
        }
    }

    // Run inference
    int result = mod_inference(features, output);

    if (result != 0) {
        // Inference error
        NPU_Reset();
        return -2;
    }

    return 0;  // Success
}

9.2.12. CCS Project Setup for NPU

1. Include NPU Support Files:

From your device SDK, add:

  • NPU driver files

  • NPU header files

  • NPU configuration files

2. Configure Linker:

Ensure linker command file includes NPU memory regions.

3. Add Compiler Defines:

Project Properties → Build → Compiler → Predefined Symbols
Add: NPU_ENABLED=1

9.2.13. Example: Arc Fault on F28P55 NPU

Complete deployment example:

Configuration:

common:
  task_type: 'generic_timeseries_classification'
  target_device: 'F28P55'

dataset:
  dataset_name: 'dc_arc_fault_example_dsk'

training:
  model_name: 'CLS_4k_NPU'
  quantization: 2
  quantization_method: 'QAT'
  quantization_weight_bitwidth: 8
  quantization_activation_bitwidth: 8

compilation:
  enable: True
  preset_name: 'compress_npu_layer_data'

Main Application:

#include "device.h"
#include "mod.h"
#include "feature_extraction.h"
#include "npu.h"

#define SAMPLE_SIZE 1024
#define FEATURE_SIZE 256
#define NUM_CLASSES 2  // Normal, Arc

float adc_buffer[SAMPLE_SIZE];
float feature_buffer[FEATURE_SIZE];
float output_buffer[NUM_CLASSES];

volatile uint8_t inference_flag = 0;

void main(void) {
    // System initialization
    Device_init();
    Device_initGPIO();

    // Initialize ADC for current sensing
    ADC_Init();

    // Initialize NPU
    NPU_Init();

    // Initialize model
    mod_init();

    // Enable interrupts
    EINT;

    while (1) {
        if (inference_flag) {
            // Extract features
            extract_features(adc_buffer, feature_buffer);

            // Run NPU inference
            mod_inference(feature_buffer, output_buffer);

            // Check for arc fault
            if (output_buffer[1] > output_buffer[0]) {
                // Arc detected!
                GPIO_writePin(ALERT_PIN, 1);
                trigger_protection();
            }

            inference_flag = 0;
        }
    }
}

__interrupt void ADC_ISR(void) {
    static uint16_t sample_idx = 0;

    adc_buffer[sample_idx++] = ADC_readResult();

    if (sample_idx >= SAMPLE_SIZE) {
        sample_idx = 0;
        inference_flag = 1;
    }

    ADC_clearInterruptStatus();
}

9.2.14. Troubleshooting NPU Issues

NPU Initialization Fails:

  • Check device is NPU-enabled

  • Verify NPU clock is enabled

  • Ensure NPU memory regions are defined

Incorrect Results:

  • Verify model is NPU-compatible

  • Check quantization settings match

  • Compare with float model on same input

NPU Hangs:

  • Check for memory conflicts

  • Verify buffer alignments

  • Reset NPU and retry

9.2.15. CCS Studio Walkthrough: F28P55x

This section provides a complete step-by-step walkthrough for deploying an arc fault classification model to the LAUNCHXL-F28P55X board using Code Composer Studio. The F28P55x device includes TI’s TINPU, so this example exercises the full NPU inference path.

Requirements

LaunchPad

LAUNCHXL-F28P55X

SDK

C2000Ware 6.00

IDE

CCS Studio 20.2.0 or later

9.2.15.1. Step 1 – Load the Example from Resource Explorer

The F28P55x arc fault example is available directly through the CCS Resource Explorer.

  1. Open Code Composer Studio.

  2. Navigate to View → Resource Explorer.

CCS Resource Explorer

Opening Resource Explorer from the View menu.

  1. In the Resource Explorer, set the Board or Device filter to LAUNCHXL-F28P55X.

  2. In the search bar, type arc_fault_dataset_validation_f28p55x.

Resource Explorer with search filters applied

Resource Explorer with board and keyword filters filled in.

  1. Select the folder arc_fault_dataset_validation_f28p55x and click Import.

Import arc fault project

Importing the arc fault project from Resource Explorer.

  1. Download and install any required dependencies when prompted.

Download dependencies dialog

Downloading required SDK dependencies.

  1. After all packages are installed the final import dialog appears. Click Finish to import the project into your workspace.

Import installed project

Final import dialog after dependencies are resolved.

9.2.15.2. Step 2 – Build the Project

  1. Go to Project → Build Project(s) (or press Ctrl+B).

Build Project menu

Building the project from the Project menu.

Verify that the build completes without errors in the Console view.

9.2.15.3. Step 3 – Set Target Configuration

  1. Switch the active target configuration from TMS320F28P550SJ9.ccxml to TMS320F28P550SJ9_LaunchPad.ccxml. Right-click the .ccxml file in Project Explorer and select Set as Active Target Configuration.

Active Target Configuration

Selecting the LaunchPad target configuration.

9.2.15.4. Step 4 – Flash the Device

  1. Connect the LAUNCHXL-F28P55X LaunchPad to your PC via USB.

  2. Go to Run → Flash Project.

Flash Project

Flashing the built project to the device.

  1. (Optional) If a firmware update prompt appears, click Update.

Firmware update dialog

Firmware update dialog – click Update if it appears.

9.2.15.5. Step 5 – Debug and Verify

  1. After flashing, the Debug perspective opens. Click the Debug icon to start a debug session.

Debug screen

CCS Debug perspective after flashing.

  1. Place a breakpoint on the line that follows the inference call in application_main.c.

Setting breakpoint

Setting a breakpoint after the inference call.

  1. Click Resume (F8) to run the program. When the breakpoint is hit, add the variable test_result to the Watch window.

Watch variable test_result

Adding test_result to the Watch window.

  1. Inspect the value:

    • test_result == 1 – model inference passed (output matches golden vector).

    • test_result == 0 – model inference failed.

test_result value

Verifying the test_result value in the Watch window.

9.2.16. Required Files from ModelMaker

The CCS example arc_fault_dataset_validation_f28p55x requires four files generated by a ModelMaker run. After ModelMaker finishes, copy each file from its ModelMaker output path to the corresponding CCS project path.

File

Purpose

ModelMaker Source Path

CCS Project Destination

mod.a

Compiled model library

.../compilation/artifacts/mod.a

ex_arc_fault_dataset_validation_f28p55x/artifacts/mod.a

tvmgen_default.h

Model inference API header

.../compilation/artifacts/tvmgen_default.h

ex_arc_fault_dataset_validation_f28p55x/artifacts/tvmgen_default.h

test_vector.c

Golden-vector test data

.../training/quantization/golden_vectors/test_vector.c

ex_arc_fault_dataset_validation_f28p55x/test_vector.c

user_input_config.h

Feature extraction config

.../training/quantization/golden_vectors/user_input_config.h

ex_arc_fault_dataset_validation_f28p55x/user_input_config.h

The ... prefix in the source paths expands to your ModelMaker data directory, for example:

tinyml-modelmaker/data/projects/dc_arc_fault_example_dsk/run/<run_name>/

After copying the four files, rebuild the CCS project, flash, and verify test_result in the debugger as described above.

9.2.17. Model Performance Profiling

Understanding inference performance is critical when deploying models to resource-constrained MCUs. This section describes how to measure inference cycle counts on the F28P55x device so you can evaluate the tradeoff between model accuracy and inference latency. Developers typically want to minimize cycles (faster inference), but reducing computation can also reduce model accuracy.

By profiling different model and input-size combinations, you can select the configuration that meets your latency budget while maintaining acceptable accuracy.

Requirements

  • Device: LAUNCHXL-F28P55X

  • C2000Ware 6.00.00.00

  • Code Composer Studio 20.2.0

Importing the Profiling Project

The example project ex_model_performance_f28p55x is not available through CCS Resource Explorer. You must manually copy it into the C2000Ware AI examples directory and import it:

  1. Copy the ex_model_performance_f28p55x project folder.

  2. Paste it into the C2000Ware AI examples path:

    C2000Ware_6_00_00_00/libraries/ai/feature_extract/c28/examples/
    
  3. In CCS, go to File -> Import Projects(s).

  4. Browse to the ex_model_performance_f28p55x folder and click Select Folder.

  5. Click Finish to import the project.

Running the Profiling Example

  1. Build the project: Project -> Build Project(s).

  2. Set the active target configuration to TMS320F28P550SJ9_LaunchPad.ccxml (matching your LAUNCHXL-F28P55X).

  3. Connect the launchpad to your system.

  4. Flash the project: Run -> Flash Project.

  5. After flashing, click the Debug icon to enter debug mode.

  6. Click Continue in the Debug Window to let the example run.

  7. Read the inference cycle count from the GEL Output window.

Required Files from ModelMaker

The CCS project ex_model_performance_f28p55x requires three files generated by ModelMaker after a training and compilation run:

File

Description

Destination in CCS Project

mod.a

Compiled model library

ex_model_performance_f28p55x/artifacts/

tvmgen_default.h

Header for model inference APIs

ex_model_performance_f28p55x/artifacts/

user_input_config.h

Model input/output size configuration

ex_model_performance_f28p55x/

After each ModelMaker run, copy these three files from the ModelMaker output into the corresponding CCS project locations, rebuild the project, flash, and debug to obtain the cycle count.

Configuring Different Models and Frame Sizes

To sweep across different configurations, edit the ModelMaker YAML configuration. The two key parameters are frame_size (which controls the input tensor dimension) and model_name (which selects the neural network architecture):

data_processing_feature_extraction:
    feature_extraction_name: 'Custom_Default'
    data_proc_transforms: ['SimpleWindow']
    frame_size: 128   # Input to the model (N,C,H,W) -> (1,1,128,1)

training:
    enable: True
    model_name: 'TimeSeries_Generic_1k_t'   # Select the model

By sweeping frame_size over values such as 128, 256, 512, and 1024 and choosing among TimeSeries_Generic_1k_t, TimeSeries_Generic_4k_t, TimeSeries_Generic_6k_t, and TimeSeries_Generic_13k_t, you can characterize the full accuracy-vs-cycles landscape for your application.

Profiling Results

The table below shows measured inference cycle counts and corresponding accuracies on the arc fault dataset. Input size is (N,C,H,W) = (1, 1, frame_size, 1) and the output size is 2 (binary classification).

Inference Cycles and Accuracy by Model and Frame Size

Model

128

256

512

1024

TimeSeries_Generic_1k_t

103,882 cycles (80.32%)

188,397 cycles (85.83%)

372,242 cycles (87.33%)

692,220 cycles (94.43%)

TimeSeries_Generic_4k_t

71,595 cycles (86.45%)

109,534 cycles (89.29%)

184,981 cycles (91.79%)

326,782 cycles (94.85%)

TimeSeries_Generic_6k_t

107,982 cycles (89.97%)

164,676 cycles (90.05%)

261,792 cycles (92.62%)

462,680 cycles (95.68%)

TimeSeries_Generic_13k_t

199,691 cycles (91.83%)

312,406 cycles (92.60%)

535,437 cycles (93.21%)

985,529 cycles (95.54%)

Key Takeaways

  • Larger models (higher parameter count) generally deliver better accuracy but consume more inference cycles.

  • Larger frame sizes improve accuracy at the cost of proportionally more cycles.

  • TimeSeries_Generic_4k_t offers the best cycles-per-accuracy ratio for smaller input sizes, making it a strong default choice when latency is constrained.

  • Use this profiling workflow to select the right model and frame size combination that fits within your application’s latency budget while meeting accuracy requirements.

9.2.18. Next Steps