7.7.14. ECG Classification
Edge AI solution for real-time ECG signal classification on the MSPM0G5187 with NPU. Classifies ECG signals into cardiac conditions for portable, low-power heart monitoring.
7.7.14.1. Overview
Cardiovascular diseases (CVDs) are the leading cause of death globally, responsible for approximately 17.9 million deaths per year. Early detection through continuous ECG monitoring significantly improves patient outcomes. However, traditional ECG analysis requires expensive medical equipment and trained professionals, limiting access to timely diagnosis.
This example demonstrates how Edge AI enables real-time cardiac classification on portable, low-power devices – without the need for cloud connectivity. By deploying a CNN-based model directly on the MSPM0G5187 microcontroller with NPU acceleration, ECG signals can be classified into multiple cardiac conditions at the point of care.
Application: Wearable health monitors, portable cardiac monitoring devices
Task Type: Time Series Classification
Primary Device: MSPM0G5187 (with NPU)
Also Supported: AM13E2, F28P55
Note
Device-specific configuration files are provided as config_<device>.yaml.
See the Available Configurations section below for details.
7.7.14.2. Key Performance Targets
Real-time ECG classification on-device
Low power consumption suitable for wearables
Greater than 95% classification accuracy
LED feedback for classification results
7.7.14.3. System Components
Hardware
MSPM0G5187 – Microcontroller with integrated NPU
AFE1594 Analog Front End – ECG signal acquisition
Software
Code Composer Studio (CCS) 12.x or later
MSPM0 SDK 2.08.00 or later
TI Edge AI Studio
7.7.14.4. Dataset Details
Dataset: ecg_classification_4class
The dataset contains ECG recordings labeled into the following classes:
Class |
Description |
|---|---|
Normal |
Healthy sinus rhythm |
Mild |
Minor cardiac abnormalities |
Other |
Other cardiac conditions |
7.7.14.5. Feature Extraction
The feature extraction pipeline for MSPM0 (preset ECG2500Input_Roundoff_1Frame)
processes the raw ECG signal as follows:
Sampling: 2500 samples per frame from the ECG input
Normalization: Signal normalization by rounding off
Framing: Single frame input to the model
data_processing_feature_extraction:
feature_extraction_name: ECG2500Input_Roundoff_1Frame
7.7.14.6. Model
ECG_55k_NPU (Default)
A CNN architecture optimized for the MSPM0G5187 NPU, with approximately 55K parameters. This model is designed for NPU-compatible inference, enabling efficient real-time classification on the target device.
Model |
Parameters |
Description |
|---|---|---|
|
~55,000 |
CNN optimized for NPU, default for MSPM0 |
Expected Accuracy: ~97%
7.7.14.7. Training Configuration
The default training hyperparameters for the MSPM0 configuration:
Parameter |
Value |
|---|---|
Batch size |
12 |
Learning rate |
0.001 |
Optimizer |
Adam |
Weight decay |
4e-5 |
Epochs |
25 |
Quantization: INT8 quantization is enabled by default for deployment.
Compilation: Uses the TI Neural Network Compiler (NNC), optimized for the MSPM0G5187 NPU.
7.7.14.8. Configuration (MSPM0)
common:
target_module: 'timeseries'
task_type: 'ecg_classification'
target_device: 'MSPM0G5187'
dataset:
dataset_name: ecg_classification_4class
data_processing_feature_extraction:
feature_extraction_name: ECG2500Input_Roundoff_1Frame
training:
model_name: ECG_55k_NPU
batch_size: 12
learning_rate: 0.001
weight_decay: 4e-5
optimizer: 'adam'
training_epochs: 25
num_gpus: 0
testing:
enable: True
compilation:
enable: True
7.7.14.9. Running the Example
# MSPM0G5187 (primary target)
cd tinyml-modelzoo
./run_tinyml_modelzoo.sh examples/ecg_classification/config_MSPM0.yaml
# AM13E2
./run_tinyml_modelzoo.sh examples/ecg_classification/config.yaml
# Anomaly detection mode
./run_tinyml_modelzoo.sh examples/ecg_classification/config_anomaly_detection.yaml
cd tinyml-modelzoo
REM MSPM0G5187 (primary target)
.\run_tinyml_modelzoo.bat examples\ecg_classification\config_MSPM0.yaml
REM AM13E2
.\run_tinyml_modelzoo.bat examples\ecg_classification\config.yaml
REM Anomaly detection mode
.\run_tinyml_modelzoo.bat examples\ecg_classification\config_anomaly_detection.yaml
7.7.14.10. Available Configurations
Config File |
Target Device |
Mode |
|---|---|---|
|
MSPM0G5187 |
Classification (4-class) |
|
AM13E2 |
Classification |
|
F28P55 |
Anomaly Detection |
7.7.14.11. Anomaly Detection Mode
A separate anomaly detection configuration is available for ECG monitoring using
the config_anomaly_detection.yaml file. This mode trains on normal ECG
recordings only and detects anomalies based on reconstruction error, which can be
useful when labeled fault data is not available.
common:
task_type: 'generic_timeseries_anomalydetection'
target_device: 'F28P55'
dataset:
dataset_name: 'ecg_ad'
training:
model_name: 'AD_Linear'
training_epochs: 200
7.7.14.12. References
7.7.14.13. See Also
Arc Fault Anomaly Detection Example – Anomaly detection tutorial