CCS Launch, Load and Run
Note
The steps on this page should be done each time EVM is power cycled or when a new CCS session is started.
Prerequisites
A quick recap of the steps that need to have been done before you proceed
Make sure you have installed CCS as mentioned in Download, Install and Setup CCS
Make sure the UART port used for console is identified as mentioned in Setup UART Terminal
Make sure you have the EVM power cable, JTAG cable, UART cable connected as shown in Cable Connections
Make sure the UART or CCS console logs on doing EVM POWER-ON indicate that SOC initialization is successful
Make sure you have built the example of interest as mentioned in Build a Hello World example
Launch CCS
Start Project-less Debug with the target configuration created with Create Target Configuration
Start Project-less Debug
You will see the AM275X target configuration in the “Threads” tab of “Debug” window as shown below
Target Configuration After Launch
Load and run example binaries
POWER-ON the EVM
Starting NULL Bootloader ...
SYSFW Firmware Version 10.0.7--v10.00.07 (Fiery Fox)
SYSFW Firmware revision 0xa
SYSFW ABI revision 4.0
INFO: Bootloader_runCpu:176: CPU mcu-r5f is initialized to 800000000 Hz !!!
INFO: Bootloader_runCpu:176: CPU a530-0 is initialized to 1400000000 Hz !!!
INFO: Bootloader_runCpu:176: CPU a530-1 is initialized to 1400000000 Hz !!!
INFO: Bootloader_runCpu:176: CPU a531-0 is initialized to 1400000000 Hz !!!
INFO: Bootloader_runCpu:176: CPU a531-1 is initialized to 1400000000 Hz !!!
INFO: Bootloader_runCpu:176: CPU c7x0-0 is initialized to 1000000000 Hz !!!
INFO: Bootloader_loadSelfCpu:229: CPU r5f0-0 is initialized to 800000000 Hz !!!
INFO: Bootloader_JumpSelfCpu:248: All done, jumping self ...
Reset the CPU
Reset CPU
Load program on the CPU
Load Program
When using makefiles to build,
In the “Load Program” dialog, select “Browse” and select the program from
examples/{example folder}/{board}/{cpu}_{os}/{compiler}as shown below for the “hello world” program.
Select Program for Makefile Build
When using CCS projects,
In the “Load Program” dialog, select “Browse Project”,
select the project and then select the program as shown below,
Select Program for CCS Projects Build
Select the Program from CCS Project
After the program is loaded, you will see the program is halted at “main” as shown below
Program at main()
Depending on the example you are running, you may need to load more programs on other CPUs for the example to work as expected. Typically, this is needed for multi-core interprocessor communication (IPC) examples. For the “hello world” program shown above, no more programs need to be loaded.
Select “Continue” to run the program and debug using the various CCS debug options
Run the Program
The program output will be seen on CCS console, and/or UART terminal, if enabled. Below shows a sample output on both CCS console and UART console, after running the “hello world” program.
Run the Program
Re-load and run example binaries
Here simply repeat the steps shows in Load and run example binaries
It is especially important to “reset the CPU” before reloading the program.
In most cases, you don’t need to power-cycle the EVM to reload the program or load a new program.
In some cases, depending on whether the previous program execution was successful or not, the CPU or some SOC peripheral may be in a exception or hang state. In this case program reload may not work.
SOLUTION: Power cycle the EVM and repeat all steps shown on this page.