Driver Porting Layer (DPL) demo

Introduction

This example shows a simple application, which setups the CPU and the underlying RTOS or no-RTOS environment on the supported SOC.

The example does the below

  • Setup a timer with system tick of 1ms, setup MPU and cache (if available)

  • Create a RTOS task (in RTOS example)

  • Trigger a ISR and signal a semaphore from ISR to main task

  • Show usage of clock delay

  • Show usage of cache APIs

  • Show usage of heap APIs

Supported Combinations

Parameter

Value

CPU + OS

r5fss0-0 nortos

CPU + OS

r5fss0-0 freertos

CPU + OS

c75ss0-0 freertos

CPU + OS

c75ss1-0 freertos

CPU + OS

wkup-r5fss0-0 freertos

Toolchain

ti-arm-clang

Toolchain

ti-c7000

Board

am275x-evm

Example folder

examples/kernel/dpl/dpl_demo/

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).

  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)

See Also

Driver Porting Layer (DPL)

Sample Output

Shown below is a sample output when the application is run,

[DPL] Hwi post ...
[DPL] Hwi post ... DONE !!!
[DPL] Sleep for 100 msecs ...
[DPL] Sleep ... DONE (Measured time = 100000 usecs, CPU cycles = 80000055 ) !!!
[DPL] Running cache operations ...
[DPL] Running cache operations ... DONE !!!
[DPL] Heap free size = 1984 bytes
[DPL] Allocated 1023 bytes @ 0x80010440, heap free size = 896 bytes
[DPL] Free'ed 1023 bytes @ 0x80010440, heap free size = 1984 bytes
All tests have passed!