MMCSD
Attention
Please note that this driver is supported only on DM R5(WKUP R5) as part SBL examples. It is not supported on MCU-R5.
Multi-Media Card Secure Digital (MMCSD) peripheral is a driver which provides an interface with storage devices which follows MMC/SD/SDIO protocol. The driver supports single bit, four bit and eight bit data lines to communicate with the connected media.
The MMCSD controller provides accessibility to external MMC/SD/SDIO devices using a programmed IO method or DMA data transfer method. There are two MMCSD modules inside the SOC - MMCSD0 ,MMCSD1 and MMCSD2.
Features Supported
MMCSD0 supports eMMC 5.1, and also backward compatible withe earlier eMMC standards
MMCSD1 supports SD card HC 4.10 and SD Physical Layer v3.01, SDIO v3.00
SysConfig Features
Note
It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.
Features not Supported
MMCSD0 does not support SD card, SDIO and voltages 3.0V and 1.2V.
MMCSD0 does not support HS400 DDR.
MMCSD1 does not support MMC card, UHS-II SD card and SDR50, DDR50 and SDR104.
The MMCSD driver doesn’t support interrupt mode.
The MMCSD driver doesn’t support 4-bit and 1-bit bus width transfers for eMMC and 1-bit bus width transfer for SD.
The default source impedance of 50 Ohms (Driver Type 0) is only supported for eMMC cards. Other driver types are not supported.
Example Usage
Include the below file to access the APIs
#include <stdio.h>
#include <drivers/mmcsd.h>
Instance Open Example
MMCSD_Params mmcsdParams;
MMCSD_Params_init(&mmcsdParams);
gMmcsdHandle = MMCSD_open(0, &mmcsdParams);
DebugP_assert(gMmcsdHandle != NULL);
Instance Close Example
MMCSD_close(gMmcsdHandle);
API Reference
Refer to the MMCSD driver header file for detailed API information.