Introduction

Welcome to FreeRTOS SDK for AM275X. This SDK contains examples, libraries and tools to develop RTOS and no-RTOS based applications for ARM R5F, TI C75 and related peripherals.

Getting Started

To get started, see Getting Started

Block Diagram

Given below is a block diagram of the SW modules in this SDK, Software Block Diagram

The main software components in the block diagram are described below

Software Components

Documentation Page

Description

OS Kernel

No RTOS

NO RTOS

Contains modules which implement no-RTOS execution environment consisting of timers, ISR, main thread. Allows software on top to run in bare metal mode.

FreeRTOS Kernel

FreeRTOS

FreeRTOS Kernel, provides a execution environment consisting of tasks, semaphores, timers, see https://www.freertos.org/RTOS.html

FreeRTOS POSIX

FreeRTOS

Limited POSIX APIs with FreeRTOS underneath, provides pthreads, mqueue, semaphore, see https://www.freertos.org/FreeRTOS-Plus/FreeRTOS_Plus_POSIX/index.html

Driver Porting Layer (DPL)

Driver Porting Layer (DPL)

APIs used by drivers to abstract the OS environment. Example, Semaphore, HW interrupts, mutex, clock.

Device Drivers and HAL (Hardware Abstraction Layer)

SOC Peripheral Drivers

SOC Peripheral Drivers

Device Drivers library and APIs for peripherals within the SOC. Example, I2C, GPIO, UART.

Board Peripheral Drivers

Board Peripheral Drivers

Device Drivers library and APIs for peripherals on the board or EVM. Example, Flash.

Software Diagnostics Library

Signal Processing

Signal Processing

Signal Processing

Supports real-time signal processing operations for embedded and high-performance applications.

Examples

Examples

Examples and Demos

Examples showing usage of different SW libraries and APIs

Tools (used on host machine)

Code Composer Studio (CCS)

Using SDK with CCS Projects

IDE used to build projects, debug programs.

TI CLANG Compiler Toolchain

TI CLANG CGT Homepage

CLANG based ARM compiler from TI for ARM R5F and MCU-R5F

TI C7000 Compiler Toolchain

TI C7000 CGT HOMEPAGE

CLANG based ARM compiler from TI for C75

SysConfig

Using SDK with SysConfig

System configuration tool, used to configure peripherals, pinmux, clocks and generate system initialization code

TI Resource Explorer (TIREX)

Using SDK with TI Resource Explorer

Web browser based tool to explore the SDK, select, import and run the examples

SDK Tools and Utilities

Tools and Utilities

Additional tools and utilities, like flashing tools, booting tools, CCS loading scripts used with the SDK development flow

Directory Structure

Given below is a overview of the directory structure to help you navigate the SDK and related tools.

Folder/Files

Description

${SDK_INSTALL_PATH}/

README_FIRST_AM275X.html

Open this file in a web browser to reach this user guide

makefile

Top level makefile to build the whole SDK using “make”

imports.mak

Top level makefile to list paths to dependent tools

docs/

Offline browseable HTML documentation

examples/

Example applications for AM275X, across multiple boards, CPUs, NO-RTOS, RTOS

source/

Device drivers, middleware libraries and APIs

tools/

Tools and utilities like CCS loading scripts, initialization scripts.

${SDK_INSTALL_PATH}/source/

board/

Board peripheral device drivers

drivers/

Soc peripheral device drivers

kernel/

NO RTOS and RTOS kernel and Driver Porting layer (DPL) for these environments.

${SDK_INSTALL_PATH}/examples/

drivers/

SOC and board level focused device drivers examples. The examples are based on both NO-RTOS and RTOS

empty/

Template projects to copy to your workarea and then modify based on your custom application needs

kernel/

NO RTOS and RTOS kernel focused examples

security/

Security focused examples

${SDK_INSTALL_PATH}/tools/

/

Additional tools and utilities used by the SDK

Given below are the paths where the different tools needed outside the SDK, like CCS, SysConfig are installed by default in Windows. In Linux, the tools are installed by default in ${HOME}/ti.

Folder/Files

Description

C:/ti/ccs2031

Code Composer Studio

C:/ti/sysconfig_1.26.2

SysConfig. NOTE, SysConfig is also installed as part of CCS at ${CCS_INSTALL_PATH}/ccs/utils/sysconfig_x.x.x

C:/ti/ti-cgt-armllvm_4.0.5.LTS

TI ARM CLANG compiler tool chain

C:/ti/ti-cgt-c7000_5.0.0.LTS

C7000 compiler tool chain

Licenses

The licensing information of this SDK, as well as any third-party components included which are made available under a number of other open-source licenses are enumerated as part of the manifest. A complete manifest along with export control information is detailed here LINK

Help and Support

For additional help and support, see https://e2e.ti.com/support/processors/f/processors-forum