HW Interrupts
Features Supported
Register a interrupt callback to a specific CPU number
Ability to pass user specific argument to the interrupt callback
Enable, disable, restore and clear specific CPU interrupts
Enable, disable, restore global CPU interrupt
For ARM R5,
Ability to specify interrupt as FIQ or IRQ, level or pulse
Ability to specify interrupt priority
Features NOT Supported
See also FreeRTOS, NO RTOS for list of unsupported features.
Important Usage Guidelines
For ARM R5,
TI VIM is the interrupt controller that is supported.
HwiP_disable,HwiP_restore,HwiP_enableonly affect state of IRQ. FIQ state is not changedRefer ARMv7-R Architecture reference manual and SOC TRM for more details.
Example Usage
Include the below file to access the APIs,
//! [include]
#include <stdio.h>
#include <kernel/dpl/HwiP.h>
//! [include]
//! [isr]
void myISR(void *args)
{
/* my ISR */
Example ISR:
//! [isr]
void samples()
{
{
//! [register]
HwiP_Params hwiParams;
HwiP_Object hwiObj;
HwiP_Params_init(&hwiParams);
/* for R5F, interrupt #10 at VIM */
hwiParams.intNum = 10;
/* for M4F, external interrupt #10 at NVIC is
16 internal interrupts + external interrupt number at NVIC
Example to register a ISR for CPU interrupt 10:
*/
/* for C75, CLEC event ID can be mapped to any of the internal interrupt number
set both event ID and interrupt number
to configure harware clec event #10
hwiParams.eventId = 10;
hwiParams.intNum = 31;
to configure software interrupt #31
hwiParams.eventId = HWIP_INVALID_EVENT_ID;
hwiParams.intNum = 31;
Example to disable and restore interrupts across a critical section:
*/
hwiParams.callback = myISR;
hwiParams.args = NULL;
HwiP_construct(&hwiObj, &hwiParams);
//! [register]
}
{
//! [disable]
uintptr_t oldIntState;
oldIntState = HwiP_disable();
/* critical section */
API Reference
Defines
-
HWIP_INVALID_EVENT_ID
-
HwiP_OBJECT_SIZE_MAX
Max size of Hwi object across no-RTOS and all OS’s.
Typedefs
-
typedef void (*HwiP_FxnCallback)(void *args)
Callback that is called when a HW interrupt is received.
- Param args:
[in] user argument passed during HwiP_construct
Functions
-
void HwiP_Params_init(HwiP_Params *params)
Set default values to HwiP_Params.
Strongly recommended to be called before seting values in HwiP_Params
- Parameters:
params – [out] parameter structure to set to default
-
int32_t HwiP_construct(HwiP_Object *obj, HwiP_Params *params)
Create a Hwi object.
- Parameters:
obj – [out] created object
params – [in] parameter structure
- Returns:
SystemP_SUCCESS on success, SystemP_FAILURE on error
-
int32_t HwiP_setArgs(HwiP_Object *obj, void *args)
Set argument to pass to the ISR.
- Parameters:
obj – [out] created object
args – [in] argument to pass to the ISR
- Returns:
SystemP_SUCCESS on success, SystemP_FAILURE on error
-
void HwiP_destruct(HwiP_Object *obj)
Cleanup, delete, destruct a Hwi object.
- Parameters:
obj – [in] Hwi object
-
void HwiP_enableInt(uint32_t intNum)
Enable a specific interrupt.
- Parameters:
intNum – [in] Interrupt number
-
uint32_t HwiP_disableInt(uint32_t intNum)
Disable a specific interrupt.
The return value is typically used with HwiP_restoreInt to restore the interrupt state to old value.
- Parameters:
intNum – [in] Interrupt number
- Returns:
old interrupt state,
0: interrupt was disabled previously,
1: interrupt was enabled previously
-
void HwiP_restoreInt(uint32_t intNum, uint32_t oldIntState)
Restore a specific interrupt.
The oldIntState value typically returned by HwiP_disableInt is used to restore the interrupt state to old value.
- Parameters:
intNum – [in] Interrupt number
oldIntState – [in] 0: disable interrupt, 1: enable interrupt
-
void HwiP_clearInt(uint32_t intNum)
Clear a pending specific interrupt.
- Parameters:
intNum – [in] Interrupt number
-
void HwiP_post(uint32_t intNum)
Force trigger a specific interrupt.
- Parameters:
intNum – [in] Interrupt number
-
uintptr_t HwiP_disable(void)
Disable all interrupts.
Note
In case of ARM R5F, ARM M4F, this only disables IRQ.
FIQ is not disabled.
In case of ARM M4F, this only disables interrupts which has priority between 1-7.- Returns:
interrupt state before disable, typically used by HwiP_restore later
-
void HwiP_enable(void)
Enable all interrupts.
Note
In case of ARM R5F, ARM M4F, this only enables IRQ.
FIQ is not enabled.
-
void HwiP_restore(uintptr_t oldIntState)
Restores all interrupts to a given state.
Note
In case of ARM R5F, ARM M4F, this only restores IRQ state.
FIQ state is not changed.
- Parameters:
oldIntState – [in] interrupt state, typically returned by HwiP_disable earlier
-
uint32_t HwiP_inISR(void)
Check if the caller of this function is inside a ISR or not.
In some cases, like with freertos, some functions cannot be called from within the OS ISR handler, this API allows the user and some driver porting layer (DPL) APIs to check and call the appropiate ISR safe API when in ISR handler mode.
To get the exact CPU mode of the executing CPU, use the low level CPU specific system calls/registers.
Note
In case of ARM R5F, this only checks if caller is not inside inside system mode or not. This means when HwiP_inISR returns 1, CPU is in IRQ mode or FIQ or abort mode. And when HwiP_inISR return 0, CPU is not in system mode.
- Returns:
0 not in interrupt mode, 1 in interrupt mode
-
void HwiP_init(void)
Initialize Hwi module.
Disables all individual interrupts
Clears all individual interrupts
Enables global interrupts
Note
MUST be called during system intialization before any HwiP_construct API calls.
Note
In case of ARM R5F, ARM M4F, this initializes and enables both FIQ and IRQ
-
int32_t HwiP_registerNmiHandler(HwiP_FxnCallback nmiHandler, void *args)
This API registers the NMI handler.
- Parameters:
nmiHandler – [in] Callback function to be called for NMI
args – [in] Args passed for the NMI callback
- Returns:
SystemP_SUCCESS on success, SystemP_FAILURE on error
-
int32_t HwiP_unregisterNmiHandler(void)
This API unregisters the current NMI handler.
- Returns:
SystemP_SUCCESS on success, SystemP_FAILURE on error
-
struct HwiP_Config
- #include <HwiP.h>
HwiP config parameters, setup as part of SysConfig, not to be set by end-users directly.
Public Members
-
uint32_t intcBaseAddr
For R5F, this is VIM base addr
-
uint32_t intcBaseAddr
-
struct HwiP_Params
- #include <HwiP.h>
Parameters passed during HwiP_construct.
Public Members
-
uint32_t intNum
CPU interrupt number.
-
HwiP_FxnCallback callback
Callback to call when interrupt is received
-
void *args
Arguments to pass to the callback
-
uint16_t eventId
Event ID to register against, only used with c6x with event combiner and c7x clec configurer
-
uint8_t priority
Interrupt priority, only used with ARM R5, ARM M4
-
uint8_t isFIQ
0: Map interrupt as ISR, 1: map interrupt as FIQ, only used with ARM R5
-
uint8_t isPulse
0: Map interrupt as level interrupt, 1: Map interrupt as pulse interrupt, only used with ARM R5, ARM M4
-
uint32_t intNum
-
struct HwiP_Object
- #include <HwiP.h>
Opaque Hwi object used with the Hwi APIs.
Public Members
-
uint32_t rsv[HwiP_OBJECT_SIZE_MAX / sizeof(uint32_t)]
reserved, should NOT be modified by end users
-
uint32_t rsv[HwiP_OBJECT_SIZE_MAX / sizeof(uint32_t)]
-
struct AIFSR
- #include <HwiP.h>
Provide additional information about data and instruction parity, ECC, and external TCM errors.
Note
Refer to ARMv7-R architecture manual for more details
-
struct IFSR
- #include <HwiP.h>
Holds status information regarding the source of the last instruction abort.
Note
Refer to ARMv7-R architecture manual for more details
-
struct ADFSR
- #include <HwiP.h>
Provide additional information about data and instruction parity, ECC, and external TCM errors.
Note
Refer to ARMv7-R architecture manual for more details
-
struct DFSR
- #include <HwiP.h>
Holds status information regarding the source of the last data abort.
Note
Refer to ARMv7-R architecture manual for more details