FreeRTOS
Note
A53 will not be available on all SOCs. All references to A53 should be ignored on such SOCs.
Introduction
FreeRTOS is a market-leading real-time operating system (RTOS) for microcontrollers and small microprocessors. Distributed freely under the MIT open source license, FreeRTOS includes a kernel and a growing set of libraries suitable for use across all industry sectors. FreeRTOS is built with an emphasis on reliability and ease of use.
FreeRTOS SDK supports FreeRTOS on below CPUS
ARM R5F
TI C75
Features Supported
FreeRTOS Kernel 11.1.0
Tasks, semaphores, mutex, queues, timers, list, heap, event groups
preemptive priority based scheduler
static and/or dynamic memory allocation mode
FreeRTOS SMP Kernel 11.1.0
Tasks, semaphores, mutex, queues, timers, list, heap, event groups
preemptive priority based scheduler for multiple cores
static and/or dynamic memory allocation mode
FreeRTOS+POSIX
Limited POSIX API wrappers on top of FreeRTOS APIs
Clock, message queue, pthread, pthread cond, pthread mutex, semaphore, timer
In order to keep the device drivers agnostic of FreeRTOS or NORTOS, additionally below Driver Porting Layer (DPL) APIs are implemented to call FreeRTOS APIs underneath,
Clock, task, semaphore, heap, cache, MPU, debug logs, HW interrupts, HW timers
Floating point save/restore with tasks (make sure to call portTASK_USES_FLOATING_POINT() before using floating point operations )
R5F ISRs,
IRQ mode,
FPU save/restore is supported.
SysConfig Features
Note
It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.
SysConfig can be used to configure below modules with FreeRTOS
Clock module, to setup system tick timer including the tick duration
Debug Log module, to select the console to use for logging as well as enable/disable logging zones
HW Timer module, to setup HW timer available on the SOC, including enabling timer interrupt and ISR registration
Features Not Supported
Co-routines, stream buffer are not enabled and are not compiled by default. Users can add these to the FreeRTOS config and makefile if they want to use these features.
Tickless IDLE mode
Task level memory protection wrapper
R5F ISRs,
FIQ mode,
nested interrupts not supported
FPU save/restore not supported.
Important files and directory structure
FreeRTOS source is distributed along with FreeRTOS SDK and given below are some important files and folders related to FreeRTOS.
| Folder/Files | Description |
|---|---|
| ${SDK_INSTALL_PATH}/source/kernel/ | |
| dpl/ | APIs to access FreeRTOS features in a OS agnostic way |
| ${SDK_INSTALL_PATH}/source/kernel/freertos | |
| lib/ | FreeRTOS library to link against. Linking to the library in this path enables the application to operate in FreeRTOS mode |
| config/ | FreeRTOS and FreeRTOS POSIX configuration header files for different CPUs within a SOC. |
| FreeRTOS-Kernel/ | FreeRTOS Kernel source code. MCU+ SDK simply clones the code from FreeRTOS github and does not modify anything in this folder |
| FreeRTOS-Kernel-smp/ | FreeRTOS Kernel source code for SMP. MCU+ SDK simply clones the code from FreeRTOS github and does not modify anything in this folder |
| FreeRTOS-POSIX/ | FreeRTOS POSIX wrapper source code. MCU+ SDK simply clones the code from FreeRTOS POSIX github and does not modify anything in this folder |
| portable/ | SDK FreeRTOS porting related files for different CPUs |
| ${SDK_INSTALL_PATH}/source/kernel/freertos/dpl | |
| common/ | FreeRTOS DPL APIs that are common across all CPUs |
| m4/ | FreeRTOS DPL APIs that are specific to M4F CPUs |
| r5/ | FreeRTOS APIs that are specific to R5F CPUs |
In addition to above files, to enable features like HW interrupts, cache, MPU, the FreeRTOS library
in FreeRTOS SDK also shares some code with NORTOS, see to makefile in the folder source\kernel\freertos to see the exact list of files
that are included to build a freertos library.
FreeRTOS usage guidelines
See FreeRTOS usage guidelines for FreeRTOS usage guidelines and comparison to SysBIOS.
Additional references
Given below are some references to learn more about FreeRTOS.
| Document Description | Web link |
|---|---|
| Easy to read FreeRTOS book | https://www.freertos.org/Documentation/RTOS_book.html |
| FreeRTOS user docs | https://www.freertos.org/features.html |
| User API reference | https://www.freertos.org/a00106.html |
| FreeRTOS core kernel source code | https://github.com/FreeRTOS/FreeRTOS-Kernel |
| FreeRTOS core kernel example source code | https://github.com/FreeRTOS/FreeRTOS/tree/master/FreeRTOS |
| Additional FreeRTOS.org maintained libraries (POSIX, TCP, Filesystem, …) | https://www.freertos.org/FreeRTOS-Labs/index.html \n https://www.freertos.org/FreeRTOS-Plus/index.html \n https://github.com/FreeRTOS |