SDL PBIST

Introduction

This example demonstrates the usage of the PBIST module. The example shows how to setup and use the PBIST controller. The example configures the algorithm and memory group. Example also prints the time taken for test execution.

Use Cases

Use Case

Description

UC-1

Configure wrong combination of algorithm and memory group.

UC-2

Configure correct combination of algorithm and memory group.

Supported Combinations

Parameter

Value

CPU + OS

r5fss0-0 nortos

Toolchain

ti-arm-clang

Board

am275x-evm

Example folder

examples/sdl/pbist/pbist_mpu/

Steps to Run the Example

See Also

PBIST

Sample Output

Shown below is a sample output when the application is run,

  PBIST Test Application

PBIST Test Application

Starting PBIST failure insertion test on Pulsar1, index 0...
 Delta Cores prep time in micro secs 327
 Delta PBIST execution time in micro secs 12
 Delta Cores restore time in micro secs 252
PBIST complete Pulsar1, test index 0

Starting PBIST failure insertion test on C7X0, index 1...
 Delta Cores prep time in micro secs 175
 Delta PBIST execution time in micro secs 14
 Delta Cores restore time in micro secs 139
PBIST complete C7X0, test index 1

Starting PBIST failure insertion test on C7X1, index 2...
 Delta Cores prep time in micro secs 175
 Delta PBIST execution time in micro secs 14
 Delta Cores restore time in micro secs 138
PBIST complete C7X1, test index 2

Starting PBIST failure insertion test on DM2, index 3...
 Delta Cores prep time in micro secs 25
 Delta PBIST execution time in micro secs 9
 Delta Cores restore time in micro secs 23
PBIST complete DM2, test index 3

Starting PBIST test on Pulsar1, index 0...
 Delta Cores prep time in micro secs 273
 Delta PBIST execution time in micro secs 519
 Delta Cores restore time in micro secs 247
PBIST complete Pulsar1, test index 0

Starting PBIST test on C7X0, index 1...
 Delta Cores prep time in micro secs 179
 Delta PBIST execution time in micro secs 6257
 Delta Cores restore time in micro secs 139
PBIST complete C7X0, test index 1

Starting PBIST test on C7X1, index 2...
 Delta Cores prep time in micro secs 179
 Delta PBIST execution time in micro secs 6256
 Delta Cores restore time in micro secs 139
PBIST complete C7X1, test index 2

Starting PBIST test on DM2, index 3...
 Delta Cores prep time in micro secs 25
 Delta PBIST execution time in micro secs 713
 Delta Cores restore time in micro secs 24
PBIST complete DM2, test index 3

PBIST Functionality Test Passed.

All tests have passed.