Configuring OptiFlash various IP
Introduction
This document gives a basic introduction to configuring different IPs, which is part of OptiFlash.
How to configure FLC.
FLC is a simplified DMA. To configure FLC, in syscfg, it can be done by clicking to the Fast Local Copy nav menu item under OptiFlash drop down menu at the bottom.
Use Add button to to add FLC instances. For am275x case, there are a total of 4 FLC instances per R5 core. All info that needs to be given is source address, destination address and size. Make sure that all these fields are 4K aligned.
How to configure RL2?
RL2 is, basically, an L2 cache controller. Highlighting the controller keyword here, because, unlike the L1 cache controller, which has internal cache memory, RL2 does not have internal cache memory. RL2 needs to be configured, and a part of On-chip SRAM needs to be assigned for RL2 cache memory.
There are three configurations that are largely needed:
Size of the L2 cache
Range of memory to cache
SRAM memory region to be used as L2 cache memory This SRAM memory region is an L2 remote region.
Before configuring RL2, 1st requirement is to allocate a part of L2 memory as cache bank. To do this:
In linker file you have to set isrl2 to true.
Make sure that size of the memory region is more than the size of the cache that is required for the application. Here, since it is required to have 128KB of application, therefore, the size of this memory region L2_CACHE_BANK has been set to 128KB.
Now once memory region has been created, RL2 can now be configured and its configuration can be done from syscfg as follows:
By selecting Layer2 Cache from the OptiFlash drop-down, the above configurations come:
Make sure the above module is enabled. This helps in enabling and disabling Layer 2 caches without losing configurations.
External Flash cached region start addressandExternal Flash cached region end addressdefine the range of addresses that need to be cached in L2 Cache.Size of cacheis the size of L2 cache that is required to be configured.