Using SDK with Makefiles
Note
The steps on this page show screen shots and description based on Linux. However the steps in Windows would remain the same, unless mentioned otherwise.
Note
In Windows, use gmake instead of make
Note
The screen shots shown on this page are for AM64x MCU+ SDK v7.3.0. You would see your specific SOC and SDK version that is installed. However the instructions and steps mentioned remain the same, unless mentioned otherwise.
Introduction
All SDK examples and libraries can be built using makefiles via command line. Using command line one can also open SysConfig GUI to configure the example. This section provides basic instructions and tips on using makefiles.
Enabling “make” in Windows
Attention
This step needs to be done once on a Windows host machine. Nothing needs to be done for Linux.
Windows, unlike Linux, does not come pre-installed with GNU make. CCS provides a GNU make executable. However the path to this GNU make executable should be visible to the windows command prompt.
To add “make” to your path environment variable do below,
Add Environment Variable
Edit the “Path” variable and add the path to C:/ti/ccs2031/ccs/utils/bin in the “Path” variable.
Confirm that you are able to see gmake in Windows by doing below
C:\ti>gmake -v
The expected output is shown below
GNU Make 4.1 Built for Windows32 Copyright (C) 1988-2014 Free Software Foundation, Inc. License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html> This is free software: you are free to change and redistribute it. There is NO WARRANTY, to the extent permitted by law.
Building Libraries with Makefiles
Note
CCS projects are not supported for libraries and if any library source file or header file is modified the libraries need to be rebuilt as shown below
When SDK is installed the drivers, FreeRTOS, NORTOS and other libraries are pre-built for both “debug” mode and “release” mode. However you can modify the library source code and rebuild all the libraries using makefiles.
To rebuild the libraries, do below,
cd ${SDK_INSTALL_PATH} make -s libs PROFILE=releaseTo clean all library generated object files and libraries, do below
cd ${SDK_INSTALL_PATH} make -s libs-clean PROFILE=release
Additionally, you can pass
PROFILE=debugto build the libraries without optimizations. This helps when debugging code in CCS debugger.
Building examples with makefiles
You can build example applications using CCS projects as well as makefiles.
To build using makefiles, firstly identify the example to build by doing below
make -s help
This will list all the make “commands” that you can execute. A sample output snippet is shown below,
# Notes, # - Use -j to invoke parallel builds # - Use PROFILE=debug or PROFILE=release [default] to build in debug or release profile # # Overall build targets, # ====================== # make -s -f makefile.{soc} help ... # Example build targets, # ====================== # make -s -C examples/hello_world/{board}/r5fss0-0_nortos/ti-arm-clang [all clean syscfg-gui syscfg] # make -s -C examples/hello_world/{board}/r5fss0-0_freertos/ti-arm-clang [all clean syscfg-gui syscfg] # make -s -C examples/hello_world/{board}/m4fss0-0_nortos/ti-arm-clang [all clean syscfg-gui syscfg] # make -s -C examples/hello_world/{board}/m4fss0-0_freertos/ti-arm-clang [all clean syscfg-gui syscfg] ... # System Example build targets, # ============================= # make -s -C examples/drivers/ipc/ipc_notify_echo/{board}/system_freertos_nortos [all clean syscfg-gui syscfg] # make -s -C examples/drivers/ipc/ipc_rpmsg_echo/{board}/system_freertos_nortos [all clean syscfg-gui syscfg] ...
All examples are arranged as below
examples/{component or module}/{optional sub-module or sub-component}/ | + -- {example name}/{board on which this example can run}/ | + -- {cpu}_{os}/{compiler toolchain}
To build a given example pick the “example combo” that you want to build and copy-paste that command on the command prompt as below
cd ${SDK_INSTALL_PATH} make -s -C examples/hello_world/{board}/m4fss0-0_freertos/ti-arm-clang all PROFILE=releaseAs shown above, one can also pass
PROFILE=releaseorPROFILE=debugto build in “release” or “debug” profile.Instead of “all” you can also pass other arguments as below.
To clean a example do,
cd ${SDK_INSTALL_PATH} make -s -C examples/hello_world/{board}/r5fss0-0_freertos/ti-arm-clang clean PROFILE=releaseTo launch SysConfig GUI from command line for a example do, (see also Using SDK with SysConfig)
cd ${SDK_INSTALL_PATH} make -s -C examples/hello_world/{board}/r5fss0-0_freertos/ti-arm-clang syscfg-guiTo simply build all examples, do below
cd ${SDK_INSTALL_PATH} make -s examples PROFILE=releaseExplore additional commands listed via
make -s helpfor more options
Building System Examples with Makefiles
Some examples, to run correctly, need multiple binaries on different CPUs to be build, loaded and run. Such examples are called “system” examples. One such example is inter-processor communication example, which shows multiple CPUs communicating among each other.
These examples are listed under
System Example build targetswhenmake -s helpis done... # System Example build targets, # ============================= # make -s -C examples/drivers/ipc/ipc_notify_echo/{board}/system_freertos_nortos [all clean syscfg-gui syscfg] # make -s -C examples/drivers/ipc/ipc_rpmsg_echo/{board}/system_freertos_nortos [all clean syscfg-gui syscfg] ...
When the command shown under “System Example …” is executed, multiple makefiles are executed to build executables for all CPUs associated with that “system” example
You can also launch SysConfig using the system example makefile as shown in below example, (see also Using SDK with SysConfig)
make -s -C examples/drivers/ipc/ipc_notify_echo/{board}/system_freertos_nortos syscfg-gui
Here SysConfig will show the configuration of all CPUs in a single SysConfig window.
SysConfig Multi-CPU View
Building the Whole SDK with Makefiles
The whole SDK can be built using makefiles by running below command,
cd ${SDK_INSTALL_PATH} make -s all PROFILE=releaseSimilarly to clean the whole SDK, do below
cd ${SDK_INSTALL_PATH} make -s clean PROFILE=release
Load and Run Executables Built with Makefiles
The generated binary from makefile is located as the below path
examples/{component or module}/{optional sub-module or sub-component}/ | + -- {example name}/{board on which this example can run}/ | + -- {cpu}_{os}/{compiler toolchain} | + -- {example_name}.release.out + -- {example_name}.debug.out + -- {example_name}.release.appimage.{device_type} + -- {example_name}.debug.appimage.{device_type}
The same folder also has .map files which have more information about the binary size and memory section used, and so on.
Tips and Tricks when working with Makefiles
In general, the makefiles are written to be simple and use very basic GNU make syntax and options. You can simply open the makefile located within a example or library folder to see the different compile options, include paths, files, include directory, pre-processor defines etc that are used to build that example or library.
The only common file included by all makefiles is the top level
${SDK_INSTALL_PATH}/imports.mak. This file defines paths to common tools like compiler, syscfg, CCS that are used by all examples. If you have installed the tools like CCS, SysConfig, Compiler at non-default paths, then modify the paths defined in this file.When a specific example is built the libraries used by it are not checked for changes i.e. dependency is not set. So make sure to do a
make -s libs PROFILE={debug or release}to build all libraries in case you have changed any library source or header file. This checks and triggers a “incremental” build across all libraries.On Linux, you can pass
-joption to allow make to use all CPUs on your host machine when running make. This will make the build time significantly faster depending on your host machine speed.On Windows, the windows command prompt sometimes locks up when make is invoked with
-joption. One solution is use a different shell in windows like the bash shell provided by GIT for windows, https://git-scm.com/download/win . With the bash shell for windows, you can pass-jto make the builds fastYou can pass
-sto build in “silent” mode. This will suppress the actual command that is executed. So if you dont pass-sthen the console will show the exact command that is executed by make. This can be useful in debugging error, if any.You can pass
PROFILE=debugorPROFILE=releaseas arguments to build in debug mode or release modeYou can also build a example by going to the example folder where the makefile is located and simply type one of below,
cd ${SDK_INSTALL_PATH}/examples/hello_world/{board}/r5fss0-0_freertos/ti-arm-clang make -s all PROFILE={debug or release} # Build the example make -s clean PROFILE={debug or release} # Clean the example make -s syscfg-gui # Launch SysConfig GUI for the exampleIn general, explore the commands and options listed under
make -s help