SBL EMMC
Introduction
This is a bootloader example, which shows an example of booting RTOS/NORTOS applications on R5, C7x and HSM cores.
The booting is done in single stage
The stage is multithreaded with one thread runs the sciServer and the other thread runs the SBL which boots the RTOS/NORTOS applications to R5/C7x/HSM cores
SBL reads the CANUART_WAKE_STAT1 MMR in wakeup control MMR to detect partial IO (or IO retention) mode exit. If exit is detected, then SBL will save the wake reason, that is the pad number that triggered the wakeup in BACKUP MMR0 of wakeup control MMR and clear isolation from the pins. Then, it continues the boot.
The SBL uses 5 appimages
tiboot3.bin with SBL, TIFS, BoardConfig
mcelf for R5
mcelf for C7x
mcelf for HSM
Supported Combinations
Parameter |
Value |
|---|---|
CPU + OS |
wkup_r5fss0-0 freertos |
Toolchain |
ti-arm-clang |
Board |
am275x-evm |
Example folder |
examples/drivers/boot/sbl_emmc |
Attention
While using device variants, please remove the cores that are not present on the device from the BOOTLOADER section of the example Syscfg
\imageStyle{sbl_emmc_syscfg_subparts.png,width:45%} \image html sbl_emmc_syscfg_subparts.png
Steps to Run the Example
Build the example
Since this is a bootloader, the example will be run every time you boot an application using this example. It is run from a eMMC boot media unlike other examples which are usually loaded with CCS. Nevertheless, you can build this example like you do for the others using makefile or build it via CCS by importing as a project.
When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see CCS_PROJECTS_PAGE).
When using makefiles to build, note the required combination and build using make command (see MAKEFILE_BUILD_PAGE)
Refer to the page BASIC_STEPS_TO_FLASH_FILES to flash this bootloader along with the application to boot.
Create HSM Appimage
Note
Change DEVICE_TYPE to HS in ${SDK_INSTALL_PATH}/devconfig/devconfig.mak and then generate HSM Appimage for HS-SE device.
::::{only} SOC_AM275X
- Create a HSM MCELF Image
- This can be done by running the makefile at {SDK_INSTALL_PATH}/tools/boot/HSMMCELFImageGen
- Refer [HSM_MCELF_IMAGE_GEN_TOOL](#hsm_mcelf_image_gen_tool) for more details
::::
::::{only} not SOC_AM275X
- Create a HSM Appimage
- This can be done by running the makefile at {SDK_INSTALL_PATH}/tools/boot/HSMAppimageGen
- Refer [HSM_APPIMAGE_GEN_TOOL](#hsm_appimage_gen_tool) for more details
::::
### Run the example
::::{only} SOC_AM275X
- This example is the SBL which needs to be flashed on the EVM flash, along with sample application images for R5, C7x and HSM.
```{note}
For HS-SE device, use **sbl_emmc_hs.cfg** as the cfg file.
Note
For HS-FS device, use sbl_emmc_hs_fs.cfg as the cfg file.
There is a default flash config file as shown below which flashes this SBL and the IPC RPMsg echo applications
${SDK_INSTALL_PATH}/tools/boot/sbl_prebuilt/{{ VAR_BOARD_NAME_LOWER }}/sbl_emmc_hs_fs.cfgMake sure IPC rpms echo application is built before running the flash script. (see IPC RPMessage Echo)
To flash to the EVM, refer to Getting Started Flash. Only when giving the flash config file, point to the
sbl_emmc_hs_fs.cfgshown above.Example, assuming SDK is installed at
C:/ti/mcu_plus_sdkand this example and IPC application is built using makefiles, and RTOS Appimage is already created, in Windows,cd C:/ti/mcu_plus_sdk/tools/boot python uart_uniflash.py -p COM13 --cfg=C:/ti/mcu_plus_sdk/tools/boot/sbl_prebuilt/{{ VAR_BOARD_NAME_LOWER }}/sbl_emmc_hs_fs.cfgIf Linux PC is used, assuming SDK is installed at
~/ti/mcu_plus_sdkcd ~/ti/mcu_plus_sdk/tools/boot python uart_uniflash.py -p /dev/ttyUSB0 --cfg=sbl_prebuilt/{{ VAR_BOARD_NAME_LOWER }}/sbl_emmc_hs_fs.cfg
Boot the EVM in eMMC boot mode.
See Also
Sample Output
After flashing and booting the EVM, you will see below output on the UART console (Complete log is not shown)
\code
Sciserver Testapp Built On: Nov 29 2024 18:43:49 Sciserver Version: v2023.11.0.0REL.MCUSDK.MM.NN.PP.bb RM_PM_HAL Version: vMM.NN.PP Starting Sciserver….. PASSED
Starting EMMC Bootloader …
SYSFW Firmware Version 10.0.8–w2024.02-am275x (Fiery SYSFW Firmware revision 0xa SYSFW ABI revision 4.0
[KPI] Boot Media : EMMC [KPI] Boot Media Clock : 166.667 MHz [KPI] Boot Image Size : 457 KB [KPI] Cores present : [KPI] TIFS init : 722us [KPI] System_init : 1801us [KPI] Board_init : 2us [KPI] FreeRtosTask Create : 255us [KPI] Drivers_open : 97us [KPI] Board_driversOpen : 0us [KPI] sciServer_init : 15043us [KPI] SBL Drivers_open : 3052us [KPI] SBL Board_driversOpen : 94us [KPI] Sciclient Get Version : 10187us [KPI] DSP 0 Image Load : 11551us [KPI] DSP 1 Image Load : 11521us [KPI] R5FSS0_0 Image Load : 5941us [KPI] R5FSS0_1 Image Load : 5807us [KPI] R5FSS1_0 Image Load : 5819us [KPI] R5FSS1_1 Image Load : 5805us [KPI] SBL Total Time Taken : 77703us
Image loading done… Starting RTOS/Baremetal applications
[IPC RPMSG ECHO] Remote Core waiting for messages from main core … !!! [IPC RPMSG ECHO] Received and echoed 10 messages … !!! All tests have passed!!
\endcode