HYPERBUS

HYPERBUS peripheral is a driver which provides an interface with storage devices which follows HYPERRAM/HYPERFLASH protocol. The driver supports single bit, four bit and eight bit data lines to communicate with the connected media.

Features Supported

  • Support for Cypress® HyperRAM

  • Up to 166 MHz maximum memory bus operation for reads

  • Low pin count interface with LVCMOS I/O pins (can be muxed with other FSS interfaces (OSPIs)) Two memory chip selects

  • Linear incrementing mode for reads and writes

  • Asynchronous bus clock

SysConfig Features

It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.

Features not Supported

  • Cache-line wrap and fixed address modes for reads or writes

  • General Purpose Output register (FSS0_HPB0_MC_GPOR) of the HBMC is not used

  • HyperFlash

  • ECC

  • OTFA

Example Usage

Include the below file to access the APIs

#include <stdio.h>
#include <drivers/hyperbus.h>

Instance Open Example


    gHyperBusHandle = HYPERBUS_open(0);
    DebugP_assert(gHyperBusHandle != NULL);

Instance Close Example

    HYPERBUS_close(gHyperBusHandle);

API

group APIs for HYPERBUS

This module contains APIs to program and use the HYPERBUS module. The APIs can be used by other drivers to get access to HYPERBUS and also by application to initiate data transfer operation.

Chip Selects

Chip selects

HYPERBUS_CS0
HYPERBUS_CS1

HYPERBUS ECC error type

HYPERBUS_ECC_1B_ERROR
HYPERBUS_ECC_2B_ERROR
HYPERBUS_ECC_WRITE_NONALIGN_ERROR
HYPERBUS_ECC_ERR_ALL

Defines

HYPERBUS_MEM_OFFSET

Memory offset for HYPERBUS controller.

HYPERBUS_MCR_CONFIGURABLE_CS_LOW_TIME

Memory Configuration Register defines.

0x1 = configurable CS# low time, 0x0 otherwise

HYPERBUS_MCR_NO_CONFIGURABLE_CS_LOW_TIME
HYPERBUS_MCR_MAXLEN_2_BYTE

Maximum Length defines.

This bit indicates maximum read/write transaction length to memory. This bit is ignored when MAXEN bit is 0. 000000000: 2 Byte [1 HyperBus CK] 000000001: 4 Byte [2 HyperBus CK] 000000010: 6 Byte [3 HyperBus CK] 111111111: 1024 Byte [512 HyperBus CK]

HYPERBUS_MCR_MAXLEN_4_BYTE
HYPERBUS_MCR_MAXLEN_6_BYTE
HYPERBUS_MCR_MAXLEN_1024_BYTE
HYPERBUS_MCR_MERGE_WRAP_INCR

Memory Configuration Register defines.

0x1 = merge WRAP and INCR, 0x0 otherwise

HYPERBUS_MCR_NO_MERGE_WRAP_INCR
HYPERBUS_MCR_ASYMM_CACHE_SUPPORT

Memory Configuration Register defines.

0x1 = asymmetry cache support, 0x0 otherwise

HYPERBUS_MCR_NO_ASYMM_CACHE_SUPPORT
HYPERBUS_MCR_MEM_SPACE

Memory Configuration Register defines.

0x0 = memory space, 0x1 = CR space

HYPERBUS_MCR_CR_SPACE
HYPERBUS_MCR_HYPERFLASH

Memory Configuration Register defines.

0x0 = HyperFlash, 0x1 = HyperRAM

HYPERBUS_MCR_HYPERRAM
HYPERBUS_MCR_WRAPSIZE_NONE

Memory Configuration Register defines.

0x0 = wrap size none, 0x1 = 64B, 0x2 = 16B, 0x3 = 32B

HYPERBUS_MCR_WRAPSIZE_64B
HYPERBUS_MCR_WRAPSIZE_16B
HYPERBUS_MCR_WRAPSIZE_32B
HYPERBUS_DMA_CH_INVALID

Invalid DMA channel index value.

HYPERBUS_FSS_FSAS_GENREGS_SYSCONFIG_ECC_ENABLE

Value to enable ECC in SYSCONFIG register.

HYPERBUS_FSS_FSAS_GENREGS_SYSCONFIG_ECC_DISABLE

Value to disable ECC in SYSCONFIG register.

HYPERBUS_FSS_FSAS_GENREGS_STATUS_RAW_ECC_WRITE_NONALIGN_ERR_MASK

Mask for write non-aligned error field in STATUS_RAW register.

HYPERBUS_FSS_FSAS_GENREGS_STATUS_RAW_ECC_WRITE_NONALIGN_ERR_SHIFT

Shift for write non-aligned error field in STATUS_RAW register.

HYPERBUS_FSS_FSAS_GENREGS_STATUS_RAW_ECC_DOUBLE_BIT_ERR_MASK

Mask for double bit error field in STATUS_RAW register.

HYPERBUS_FSS_FSAS_GENREGS_STATUS_RAW_ECC_DOUBLE_BIT_ERR_SHIFT

Shift for double bit error field in STATUS_RAW register.

HYPERBUS_FSS_FSAS_GENREGS_STATUS_RAW_ECC_SINGLE_BIT_ERR_MASK

Mask for single bit error field in STATUS_RAW register.

HYPERBUS_FSS_FSAS_GENREGS_STATUS_RAW_ECC_SINGLE_BIT_ERR_SHIFT

Shift for single bit error field in STATUS_RAW register.

HYPERBUS_FSS_FSAS_GENREGS_ERR_ECC_TYPE_OFFSET

Offset of ECC error type register in Hyperbus FSS module.

HYPERBUS_FSS_FSAS_GENREGS_ERR_WRT_TYPE_OFFSET

Offset of write error type register in Hyperbus FSS module.

HYPERBUS_FSS_FSAS_GENREGS_ECC_ERR_CLEAR_VALUE

Value to clear ECC error in Hyperbus FSS module.

HYPERBUS_FSS_FSAS_GENREGS_IRQ_EOI_OFFSET

Offset of EOI register in Hyperbus FSS module.

HYPERBUS_FSS_FSAS_GENREGS_IRQ_EOI_VECTOR

Value to write to EOI register to clear interrupt in Hyperbus FSS module.

HYPERBUS_FSS_FSAS_GENREGS_STATUS_RAW_OFFSET

Offset of STATUS_RAW register in Hyperbus FSS module.

HYPERBUS_FSS_FSAS_GENREGS_IRQ_STATUS_OFFSET

Offset of IRQ status register in Hyperbus FSS module.

HYPERBUS_FSS_FSAS_GENREGS_IRQ_ENABLE_SET_OFFSET

Offset of IRQ enable set register in Hyperbus FSS module.

HYPERBUS_FSS_FSAS_GENREGS_IRQ_ENABLE_CLR_OFFSET

Offset of IRQ enable clear register in Hyperbus FSS module.

HYPERBUS_FSS_FSAS_GENREGS_IRQ_ENABLE_SET_VALUE

Value to write to IRQ enable set register to enable interrupts in Hyperbus FSS module.

HYPERBUS_FSS_FSAS_GENREGS_IRQ_ENABLE_CLR_VALUE

Value to write to IRQ enable clear register to disable interrupts in Hyperbus FSS module.

HYPERBUS_FSS_FSAS_ECC_REGION_START_OFFSET

Offset of ECC region start address register in Hyperbus FSS module.

HYPERBUS_FSS_FSAS_ECC_REGION_SIZE_OFFSET

Offset of ECC region size register in Hyperbus FSS module.

HYPERBUS_FSS_FSAS_ECC_REGION_OFFSET_STEP

Offset step to access ECC region start address and size registers.

HYPERBUS_FSS_FSAS_ECC_REGION_START_ADDR_SHIFT

Shift value to get ECC region start address in 4KBytes steps.

The offset is a 32-bit value that is divided by 4KBytes (0x1000). The result is the start address of the ECC region.

0x0 means the start address is 0 and the region is disabled 0x1 means the start address is 4KBytes 0xA means the start address is 40KBytes 0xF_FFFF means the start address is 4GBytes

HYPERBUS_FSS_FSAS_ECC_REGION_SIZE_SHIFT

Shift value to get ECC region size in 4KBytes steps.

The size is a 32-bit value that is divided by 4KBytes (0x1000). The result is the size of the ECC region.

0x0 means the size is 0 and the region is disabled 0x1 means the size is 4KBytes 0xA means the size is 40KBytes 0xF_FFFF means the size is 4GBytes

HYPERBUS_FSS_FSAS_NUM_ECC_REGIONS

Number of ECC regions supported by the Hyperbus FSS module.

HYPERBUS_FSS_FSAS_ECC_REGION0

First ECC region in Hyperbus FSS module (region 0)

Used to specify the first ECC region when configuring or selecting regions for ECC operations.

HYPERBUS_FSS_FSAS_ECC_REGION1

Second ECC region in Hyperbus FSS module (region 1)

Used to specify the second ECC region when configuring or selecting regions for ECC operations.

HYPERBUS_FSS_FSAS_ECC_REGION2

Third ECC region in Hyperbus FSS module (region 2)

Used to specify the third ECC region when configuring or selecting regions for ECC operations.

HYPERBUS_FSS_FSAS_ECC_REGION3

Fourth ECC region in Hyperbus FSS module (region 3)

Used to specify the fourth ECC region when configuring or selecting regions for ECC operations.

Typedefs

typedef void *HYPERBUS_Handle

A handle that is returned from a HYPERBUS_open() call.

typedef void (*HYPERBUS_ECCCallbackFxn)(HYPERBUS_Handle hyperbusHandle, uint8_t errorType)

The definition of a callback function used by the HYPERBUS driver when ECC error interrupts occur.

Param hyperbusHandle:

HYPERBUS_Handle

Param errorType:

Type of ECC error that occurred

Enums

enum HYPERBUS_Devicetype

Enum for device type.

Values:

enumerator HYPERBUS_DEVICETYPE_HYPERRAM
enumerator HYPERBUS_DEVICETYPE_NONE
enumerator HYPERBUS_DEVICETYPE_HYPERFLASH

Functions

void HYPERBUS_init(void)

This function initializes the HYPERBUS module.

void HYPERBUS_deinit(void)

This function de-initializes the HYPERBUS module.

HYPERBUS_Handle HYPERBUS_open(uint32_t index)

This function opens a given HYPERBUS peripheral.

See also

HYPERBUS_init()

See also

HYPERBUS_close()

Parameters:

index – Index of config to use in the HYPERBUS_Config array

Pre:

HYPERBUS controller has been initialized using HYPERBUS_init()

Returns:

A HYPERBUS_Handle on success or a NULL on an error or if it has been opened already

void HYPERBUS_close(HYPERBUS_Handle handle)

Function to close a HYPERBUS peripheral specified by the HYPERBUS handle.

See also

HYPERBUS_open()

Parameters:

handle – HYPERBUS_Handle returned from HYPERBUS_open()

Pre:

HYPERBUS_open() has to be called first

HYPERBUS_Handle HYPERBUS_getHandle(uint32_t index)

This function returns the handle of an open HYPERBUS Instance from the instance index.

See also

HYPERBUS_init()

See also

HYPERBUS_open()

Parameters:

index – Index of config to use in the HYPERBUS_Config array

Pre:

HYPERBUS controller has been opened using HYPERBUS_open()

Returns:

An HYPERBUS_Handle if it has been opened already or NULL otherwise

uint32_t HYPERBUS_getHyperBusDataBaseAddr(HYPERBUS_Handle handle)

This function gets the SOC mapped data base address of the HyperRam.

Parameters:

handle – An HYPERBUS_Handle returned from an HYPERBUS_open()

Pre:

HYPERBUS controller has been opened using HYPERBUS_open()

Returns:

Data BaseAddress of the HyperRam

static uint32_t HYPERBUS_makeMemCfg(HYPERBUS_Handle handle, HYPERBUS_MemCfg *pHyperBusMemCfg)

This function returns the memory configuration of the HYPERBUS Instance.

Parameters:
Pre:

HYPERBUS controller has been opened using HYPERBUS_open()

Returns:

memory configuration of the HYPERBUS Instance

static uint32_t HYPERBUS_makeMemTiming(HYPERBUS_Handle handle, HYPERBUS_MemTiming *pHyperBusMemTiming)

This function returns the memory Timings of the HYPERBUS Instance.

Parameters:
Pre:

HYPERBUS controller has been opened using HYPERBUS_open()

Returns:

memory Timings of the HYPERBUS Instance

static void HYPERBUS_isr(void *args)

This function is called by the HwiP module to service interrupts generated by the FSS of the HYPERBUS controller.

Parameters:

args – Pointer to the HYPERBUS_Config structure associated with the interrupting HYPERBUS peripheral

int32_t HYPERBUS_configureECC(HYPERBUS_Handle handle)

This function configures the ECC regions for the HYPERBUS Instance.

Parameters:

handle – An HYPERBUS_Handle returned from an HYPERBUS_open()

Pre:

HYPERBUS controller has been opened using HYPERBUS_open()

Returns:

0 on success else a negative value

int32_t HYPERBUS_setECCRegion(HYPERBUS_Handle handle, uint8_t region)

This function sets the ECC region for the HYPERBUS Instance.

Parameters:
Pre:

HYPERBUS controller has been opened using HYPERBUS_open()

Returns:

0 on success else a negative value

int32_t HYPERBUS_enableECC(HYPERBUS_Handle handle, uint8_t enableFlag)

This function enables or disables ECC for the HYPERBUS Instance.

Parameters:
Pre:

HYPERBUS controller has been opened using HYPERBUS_open()

Returns:

0 on success else a negative value

int32_t HYPERBUS_clearECCError(HYPERBUS_Handle handle, uint8_t errorType)

This function clears the ECC error for the HYPERBUS Instance.

Parameters:
  • handle – An HYPERBUS_Handle returned from an HYPERBUS_open()

  • errorType – Type of error to clear, value should be one of the HYPERBUS_ECC_ERROR_TYPE defines

Pre:

HYPERBUS controller has been opened using HYPERBUS_open()

Returns:

0 on success else a negative value

int32_t HYPERBUS_getECCErrorInfo(HYPERBUS_Handle handle, HYPERBUS_ECCErrorInfo *ECCErrorInfo)

This function returns the ECC error information for the HYPERBUS Instance.

Parameters:
Pre:

HYPERBUS controller has been opened using HYPERBUS_open()

Returns:

0 on success else a negative value

Variables

HYPERBUS_Config gHyperBusConfig[]

Externally defined driver configuration array.

uint32_t gHyperBusConfigNum

Externally defined driver configuration array size.

HYPERBUS_ECCRegion gHyperBusEccRegion[HYPERBUS_FSS_FSAS_NUM_ECC_REGIONS]
struct HYPERBUS_ECCErrorInfo
#include <hyperbus.h>

ECC Error Information structure.

This structure provides information about the ECC error

struct HYPERBUS_ECCRegions
#include <hyperbus.h>

ECC region The structure specifies the ECC region start address and size.

struct HYPERBUS_ECCRegion
#include <hyperbus.h>

Structure containing ECC region params.

struct HYPERBUS_MemCfg
#include <hyperbus.h>

Memory Configuration Structure.

This structure holds the memory configuration settings for the HYPERBUS.

struct HYPERBUS_fssDataIf
#include <hyperbus.h>

FSS Data Interface Structure.

This structure contains the global and local addresses of the data interface

struct HYPERBUS_fssHandle
#include <hyperbus.h>

FSS Handle Structure.

This structure contains the base addresses of the configuration and data interface

struct HYPERBUS_MemTiming
#include <hyperbus.h>

Register structure for the Memory Timing Register.

struct HYPERBUS_Params
#include <hyperbus.h>

HYPERBUS Parameters.

HYPERBUS Parameters are used to with the HYPERBUS_open() call.

struct HYPERBUS_Attrs
#include <hyperbus.h>

HYPERBUS instance attributes - used during init time.

struct HYPERBUS_Object
#include <hyperbus.h>

HYPERBUS driver object.

struct HYPERBUS_Config
#include <hyperbus.h>

HYPERBUS driver configuration structure.

This structure is used to pass configuration information to the HYPERBUS driver.