I2C Read

Introduction

This example demonstrates reading data from I2C based EEPROM devices present in the board. Application reads 20 samples from the EEPROM and exits.

Attention

For AM275-EVM, Board ID EEPROM address is 0x51u.

SCL and SDA pins of MCU_I2C0 are available at the MCU_HEADER in the board. MCU_I2C0 can be connected to Board ID EEPROM through making the following jumper connections as shown in the image. - Connect Pin 21 of J9 (MCU_I2C0_SDA) to Pin 27 of J3. - Connect Pin 24 of J9 (MCU_I2C0_SCL) to Pin 28 of J3.

 ```{figure} ../../images/am275x/i2c_read_am275x.png
 :align: center

 **JUMPER CONNECTIONS FOR I2C**
 ```

Supported Combinations

Parameter

Value

CPU + OS

r5fss0-0 freertos

CPU + OS

r5fss0-0 nortos

CPU + OS

c75ss0-0 freertos

Toolchain

ti-arm-clang

Toolchain

ti-c7000

Boards

am275x-evm

Example folder

examples/drivers/i2c/i2c_read

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).

  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)

See Also

I2C

Sample Output

Shown below is a sample output when the application is run,

[I2C] Read data ... !!!
[I2C] Sample 0: 255
[I2C] Sample 1: 255
[I2C] Sample 2: 255
[I2C] Sample 3: 255
[I2C] Sample 4: 255
[I2C] Sample 5: 255
[I2C] Sample 6: 255
[I2C] Sample 7: 255
[I2C] Sample 8: 255
[I2C] Sample 9: 255
[I2C] Sample 10: 255
[I2C] Sample 11: 255
[I2C] Sample 12: 255
[I2C] Sample 13: 255
[I2C] Sample 14: 255
[I2C] Sample 15: 255
[I2C] Sample 16: 255
[I2C] Sample 17: 255
[I2C] Sample 18: 255
[I2C] Sample 19: 255
[I2C] Read data ... DONE !!!All tests have passed!!