SDL MCRC Auto

Introduction

This example demonstrates the usage of the MCRC module. The example shows how to setup and use the MCRC controller in the auto mode of operation. Shows the generation of matching CRC as well as non-matching signature due to insertion of error in the block of information on which the CRC is being performed or in the signature provided to the PSA Signature Register (or both, depending on the mode).

Use Cases

Use Case

Description

UC-1

Auto-mode signature compute for Channel 1 and comparison against known value.

UC-2

Auto-mode signature compute for Channel 2 and comparison against known value.

Supported Combinations

Parameter

Value

CPU + OS

r5fss0-0 nortos

Toolchain

ti-arm-clang

Board

am275x-evm

Example folder

examples/sdl/mcrc/mcrc_auto/

Steps to Run the Example

See Also

MCRC

Sample Output

Shown below is a sample output when the application is run,

[MAIN_Cortex_R5_0_0] Sciclient direct init..... SUCCESS

MCRC Test Application

MCRC Auto mode : starting

MCRC AUTO mode on Channel 1: Transfer Test Started...

Calculating Reference MCRC signature Value.
MCRC signature value : 0x474b7cf03d4145dU
MCRC Full Mode Computation Time: 1095us

Sector signature matches - Passed
Calculated MCRC signature value : 0x474b7cf003d4145dU

UDMA Data transfer completed !!
MCRC Auto Mode Computation Time: 1095us

MCRC AUTO mode on Channel 2: Transfer Test Started...

Using Pre-Defined Reference MCRC signature Value.

Pre-defined MCRC signature value : 0x474b7cf03d4145dU

Sector signature matches - Passed
Calculated MCRC signature value : 0x474b7cf003d4145dU

UDMA Data transfer completed !!
MCRC Auto Mode Computation Time: 1095us

Test Name: MCRCAuto_main  PASSED

All tests have passed.