TIOVX User Guide
|
Interface to object descriptor. More...
Go to the source code of this file.
Data Structures | |
struct | tivx_remap_point_t |
Remap point in remap table. More... | |
struct | tivx_obj_desc_t |
Object descriptor. More... | |
struct | tivx_obj_desc_node_t |
Node object descriptor. More... | |
struct | tivx_obj_desc_image_t |
Image object descriptor as placed in shared memory. More... | |
struct | tivx_obj_desc_remap_t |
Remap object descriptor as placed in shared memory. More... | |
struct | tivx_obj_desc_matrix_t |
matrix object descriptor as placed in shared memory More... | |
struct | tivx_obj_desc_lut_t |
lut object descriptor as placed in shared memory More... | |
struct | tivx_obj_desc_pyramid_t |
pyramid object descriptor as placed in shared memory More... | |
struct | tivx_obj_desc_convolution_t |
convolution object descriptor as placed in shared memory More... | |
struct | tivx_obj_desc_threshold_t |
threshold object descriptor as placed in shared memory More... | |
struct | tivx_obj_desc_distribution_t |
distribution object descriptor as placed in shared memory More... | |
struct | tivx_obj_desc_array_t |
array object descriptor as placed in shared memory More... | |
struct | tivx_obj_desc_user_data_object_t |
user data object descriptor as placed in shared memory More... | |
struct | tivx_obj_desc_raw_image_t |
raw image descriptor as placed in shared memory More... | |
struct | tivx_obj_desc_object_array_t |
object array object descriptor as placed in shared memory More... | |
struct | tivx_obj_desc_scalar_t |
Scalar object descriptor as placed in shared memory. More... | |
struct | tivx_obj_desc_tensor_t |
Tensor object descriptor as placed in shared memory. More... | |
Macros | |
#define | TIVX_OBJ_DESC_MAX_SHM_ENTRY_SIZE (1024U) |
Macro to check max shared mem entry size. | |
#define | TIVX_IMAGE_MAX_PLANES (4u) |
Max possible planes of data in an image. | |
#define | TIVX_CONTEXT_MAX_TENSOR_DIMS (4) |
Max possible dimensions of data in a tensor. | |
#define | TIVX_REF_FLAG_LOG_RT_TRACE (0x00000001u) |
Flag to indicate if run-time trace should be logged. | |
#define | TIVX_REF_FLAG_IS_INVALID (0x00000002u) |
Flag to indicate if ref is invalid. | |
#define | TIVX_NODE_FLAG_IS_REPLICATED (0x00000001u) |
Flag to indicate if node is replicated. | |
#define | TIVX_NODE_FLAG_IS_EXECUTED (0x00000002u) |
Flag to indicate if node is executed. | |
#define | TIVX_NODE_FLAG_IS_USER_CALLBACK (0x00000004u) |
Flag to indicate if user callback is requested after node complete. | |
#define | TIVX_NODE_FLAG_IS_TARGET_KERNEL (0x00000008u) |
Flag to indicate if kernel associated with this node is a user kernel or target kernel. | |
#define | TIVX_NODE_FLAG_IS_SUPERNODE (0x00000010u) |
Flag to indicate if this node is a supernode. | |
#define | TIVX_NODE_OBJ_DESC_STATE_IDLE (0x0u) |
State of a node object descriptor to indicate it is IDLE. | |
#define | TIVX_NODE_OBJ_DESC_STATE_BLOCKED (0x1u) |
State of a node object descriptor to indicate it is BLOCKED. More... | |
#define | TIVX_OBJ_DESC_MAX_HOST_PORT_ID_CPU (16u) |
Max size of the array host_port_id, in tivx_obj_desc_t. | |
Enumerations | |
enum | tivx_obj_desc_type_e { TIVX_OBJ_DESC_IMAGE = 0x0, TIVX_OBJ_DESC_SCALAR = 0x1, TIVX_OBJ_DESC_REMAP = 0x2, TIVX_OBJ_DESC_NODE = 0x3, TIVX_OBJ_DESC_CMD = 0x4, TIVX_OBJ_DESC_MATRIX = 0x5, TIVX_OBJ_DESC_LUT = 0x6, TIVX_OBJ_DESC_CONVOLUTION = 0x7, TIVX_OBJ_DESC_DISTRIBUTION = 0x8, TIVX_OBJ_DESC_THRESHOLD = 0x9, TIVX_OBJ_DESC_ARRAY = 0xA, TIVX_OBJ_DESC_PYRAMID = 0xB, TIVX_OBJ_DESC_OBJARRAY = 0xC, TIVX_OBJ_DESC_KERNEL_NAME = 0xD, TIVX_OBJ_DESC_QUEUE = 0xE, TIVX_OBJ_DESC_DATA_REF_Q = 0xF, TIVX_OBJ_DESC_GRAPH = 0x10, TIVX_OBJ_DESC_TENSOR = 0x11, TIVX_OBJ_DESC_USER_DATA_OBJECT = 0x12, TIVX_OBJ_DESC_RAW_IMAGE = 0x13, TIVX_OBJ_DESC_SUPER_NODE = 0x14, TIVX_OBJ_DESC_INVALID = 0xFFFFu } |
Enum that list all possible object descriptor type's. More... | |
enum | tivx_image_create_type_e { TIVX_IMAGE_NORMAL, TIVX_IMAGE_UNIFORM, TIVX_IMAGE_VIRTUAL, TIVX_IMAGE_FROM_HANDLE, TIVX_IMAGE_FROM_ROI, TIVX_IMAGE_FROM_CHANNEL } |
Method by which image is created. More... | |
Functions | |
void | tivxGetObjDescList (volatile uint16_t obj_desc_id[], tivx_obj_desc_t *obj_desc[], uint32_t num_desc_id) |
Function to get the pointer to object descriptors for the given object descriptor id. More... | |
tivx_obj_desc_t * | tivxGetObjDescElement (tivx_obj_desc_t *obj_desc, uint16_t elem_idx) |
Function to get the pointer to an element of an object array. If the object being passed is a regular object descriptor then a pointer to the object is returned. More... | |
void | tivx_obj_desc_strncpy (volatile void *dst, volatile void *src, uint32_t size) |
Utility function for memory/string copy/set operation on object descriptor pointers. More... | |
void | tivx_obj_desc_memcpy (volatile void *dst, volatile void *src, uint32_t size) |
Utility function for memory/string copy/set operation on object descriptor pointers. More... | |
void | tivx_obj_desc_memset (volatile void *dst, uint8_t val, uint32_t size) |
Utility function for memory/string copy/set operation on object descriptor pointers. More... | |
int32_t | tivx_obj_desc_strncmp (volatile void *dst, volatile void *src, uint32_t size) |
Utility function for memory/string compare operation on object descriptor pointers. More... | |
int32_t | tivx_obj_desc_strncmp_delim (volatile void *dst, volatile void *src, uint32_t size, char delim) |
Utility function for memory/string compare operation on object descriptor pointers with delimiter. More... | |
Interface to object descriptor.
Definition in file tivx_obj_desc.h.