TIOVX User Guide

distribution object descriptor as placed in shared memory More...

#include <tivx_obj_desc.h>

Data Fields

tivx_obj_desc_t base
 base object descriptor
 
tivx_shared_mem_ptr_t mem_ptr
 distribution memory address
 
volatile uint32_t num_bins
 number of rows
 
volatile uint32_t offset
 number of columns
 
volatile uint32_t range
 scale factor
 
volatile uint32_t num_win
 number of windows
 
volatile uint32_t mem_size
 size of buffer pointed to by mem_ptr
 

Detailed Description

distribution object descriptor as placed in shared memory

Definition at line 686 of file tivx_obj_desc.h.


The documentation for this struct was generated from the following file: