![]() |
TIOVX User Guide
|
Object descriptor. More...
#include <tivx_obj_desc.h>
Data Fields | |
| volatile uint16_t | obj_desc_id |
| ID of object in shared memory. | |
| volatile uint16_t | type |
| Type of object descriptor, see tivx_obj_desc_type_e. | |
| volatile uint16_t | scope_obj_desc_id |
| object descriptor ID of the scope in which this object is created For element of pyramid and object array, this is obj_desc_id of encompassing pyramid, object array | |
| volatile uint16_t | in_node_done_cnt |
| number of input nodes that have consumed this obj_desc, used in pipelining mode only for data references | |
| volatile uint64_t | host_ref |
| Host reference, accessible only on HOST side. | |
| volatile uint32_t | flags |
| reference flags | |
| volatile uint32_t | element_idx |
| holds the index ID in the case that this is an element within a pyramid or object array | |
| volatile uint64_t | timestamp |
| reference timestamp | |
| volatile uint32_t | host_cpu_id |
| holds the CPU ID of the OpenVX host for this object descriptor | |
| volatile uint16_t | num_enqueues |
| holds the count of the number of times this reference has been enqueued and not dequeued | |
| volatile uint16_t | supp_data_id |
| ID of supplementary data object descriptor in shared memory. | |
| volatile uint16_t | host_port_id [TIVX_OBJ_DESC_MAX_HOST_PORT_ID_CPU] |
| holds the index of the IPC port on OpenVX host for this object descriptor for each remote CPU More... | |
Object descriptor.
Must be first element of any objects descriptors placed in shared memory
Make sure this structure is multiple of 64b
Definition at line 323 of file tivx_obj_desc.h.
| volatile uint16_t tivx_obj_desc_t::host_port_id[TIVX_OBJ_DESC_MAX_HOST_PORT_ID_CPU] |
holds the index of the IPC port on OpenVX host for this object descriptor for each remote CPU
A connection to each remote CPU could be on a different host_port_id, hence this needs to hold host_port_id for each remote CPU, this array is indexed by TIOVX CPU ID. TIVX_OBJ_DESC_MAX_HOST_PORT_ID_CPU MUST be <= TIVX_CPU_ID_MAX
Definition at line 367 of file tivx_obj_desc.h.