TIOVX User Guide

user data object descriptor as placed in shared memory More...

#include <tivx_obj_desc.h>

Data Fields

tivx_obj_desc_t base
 base object descriptor
 
tivx_shared_mem_ptr_t mem_ptr
 user data object memory address
 
volatile uint32_t mem_size
 size of buffer pointed to by mem_ptr
 
volatile uint32_t valid_mem_size
 size of valid data within the buffer
 
volatile vx_char type_name [VX_MAX_REFERENCE_NAME]
 The type name of the user data object.
 

Detailed Description

user data object descriptor as placed in shared memory

Definition at line 734 of file tivx_obj_desc.h.


The documentation for this struct was generated from the following file: