TIOVX User Guide

lut object descriptor as placed in shared memory More...

#include <tivx_obj_desc.h>

Data Fields

tivx_obj_desc_t base
 base object descriptor
 
tivx_shared_mem_ptr_t mem_ptr
 lut memory address
 
volatile vx_enum item_type
 The item type of the lut.
 
volatile vx_uint32 item_size
 size of each item
 
volatile vx_uint32 num_items
 number of items
 
volatile uint32_t mem_size
 size of buffer pointed to by mem_ptr
 

Detailed Description

lut object descriptor as placed in shared memory

Definition at line 595 of file tivx_obj_desc.h.


The documentation for this struct was generated from the following file: