TIOVX User Guide
|
Node object descriptor. More...
#include <tivx_obj_desc.h>
Data Fields | |
tivx_obj_desc_t | base |
base object descriptor | |
volatile uint32_t | flags |
node flags see TIVX_NODE_FLAG_xxx | |
volatile uint32_t | kernel_id |
ID of kernel to execute on target. | |
volatile uint32_t | kernel_name_obj_desc_id |
kernel name object descriptor ID | |
volatile uint32_t | target_id |
ID of target to execute on. Set by host. | |
volatile uint32_t | node_complete_cmd_obj_desc_id |
command to send when node completes execution More... | |
volatile uint32_t | target_kernel_index [TIVX_NODE_MAX_REPLICATE] |
Index in target kernel table. More... | |
volatile uint32_t | exe_status |
node execution status | |
volatile uint32_t | exe_time_beg_h |
node execution time | |
volatile uint32_t | exe_time_beg_l |
node execution time | |
volatile uint32_t | exe_time_end_h |
node execution time | |
volatile uint32_t | exe_time_end_l |
node execution time | |
volatile uint32_t | num_params |
number of parameters associated with this node | |
volatile uint32_t | num_out_nodes |
Number of nodes that are connected to output of this node. | |
volatile uint32_t | num_in_nodes |
Number of nodes that are connected to input of this node. | |
vx_border_t | border_mode |
border mode | |
volatile uint32_t | is_prm_replicated |
bitmask which indicates if prm is replicated valid only when TIVX_NODE_FLAG_IS_REPLICATED is set in flags. bitN = 1 means param at index N is replicated | |
volatile uint32_t | num_of_replicas |
number of times node is replicated valid only when TIVX_NODE_FLAG_IS_REPLICATED is set in flags. | |
volatile uint16_t | data_id [TIVX_KERNEL_MAX_PARAMS] |
parameter object descriptors | |
volatile uint16_t | data_ref_q_id [TIVX_KERNEL_MAX_PARAMS] |
parameter data ref q object descriptors, valid only when is_prm_data_ref_q is set | |
volatile uint16_t | out_node_id [TIVX_NODE_MAX_OUT_NODES] |
parameter object descriptors | |
volatile uint16_t | in_node_id [TIVX_NODE_MAX_IN_NODES] |
parameter object descriptors | |
volatile uint16_t | state |
node state one of TIVX_NODE_OBJ_DESC_STATE_IDLE, TIVX_NODE_OBJ_DESC_STATE_BLOCKED | |
volatile uint16_t | blocked_node_id |
node ID that is blocked on this node to be IDLE | |
volatile uint16_t | pipeline_id |
pipeline ID to which this node obj desc belongs | |
volatile uint16_t | prev_pipe_node_id |
node in the previous pipeline relative to this node | |
volatile uint32_t | is_prm_input |
bitmask which indicates if prm is input to a node bitN = 1 means param at index N is input to node | |
volatile uint32_t | is_prm_data_ref_q |
bitmask which indicates if prm is data ref q bitN = 1 means param at index N is data ref q | |
volatile uint32_t | is_prm_array_element |
bitmask which indicates if prm is array element bitN = 1 means param at index N is array element | |
volatile uint32_t | source_state |
Flag indicating whether or not node is in pipeup state or steady state. | |
volatile uint32_t | num_pipeup_bufs |
number of buffers required for pipeup state | |
volatile uint32_t | pipeup_buf_idx |
Pipe buf idx used for when to begin graph processing on source node. | |
volatile uint32_t | block_width |
variable to store the tile width for the given node | |
volatile uint32_t | block_height |
variable to store the tile height for the given node | |
Node object descriptor.
Fields with name target_* are only accessed by target CPU Fields with name host_* are only accessed by host CPU Other fields are accessed by both target and host
Definition at line 347 of file tivx_obj_desc.h.
volatile uint32_t tivx_obj_desc_node_t::node_complete_cmd_obj_desc_id |
command to send when node completes execution
This is set by host in following conditions
Definition at line 374 of file tivx_obj_desc.h.
volatile uint32_t tivx_obj_desc_node_t::target_kernel_index[TIVX_NODE_MAX_REPLICATE] |
Index in target kernel table.
Used for fast indexing to kernel functions during graph execute phase.
This is filled by target side during node create phase
Definition at line 383 of file tivx_obj_desc.h.