TIOVX User Guide

raw image descriptor as placed in shared memory More...

#include <tivx_obj_desc.h>

Data Fields

tivx_obj_desc_t base
 base object descriptor
 
tivx_shared_mem_ptr_t mem_ptr [TIVX_RAW_IMAGE_MAX_EXPOSURES]
 allocated buffer addresses (max 1 for each combined image and meta data)
 
tivx_shared_mem_ptr_t img_ptr [TIVX_RAW_IMAGE_MAX_EXPOSURES]
 image data buffer addresses
 
tivx_shared_mem_ptr_t meta_before_ptr [TIVX_RAW_IMAGE_MAX_EXPOSURES]
 meta before buffer addresses
 
tivx_shared_mem_ptr_t meta_after_ptr [TIVX_RAW_IMAGE_MAX_EXPOSURES]
 meta after buffer addresses
 
tivx_raw_image_create_params_t params
 create parameters for raw image
 
volatile uint32_t mem_size [TIVX_RAW_IMAGE_MAX_EXPOSURES]
 image plane buffer size
 
volatile uint32_t create_type
 method by which raw image was created, see tivx_image_create_type_e
 
vx_imagepatch_addressing_t imagepatch_addr [TIVX_RAW_IMAGE_MAX_EXPOSURES]
 raw image exposure addressing parameters
 
vx_rectangle_t valid_roi
 valid region of raw image to use for processing
 

Detailed Description

raw image descriptor as placed in shared memory

Definition at line 754 of file tivx_obj_desc.h.


The documentation for this struct was generated from the following file: