TIOVX User Guide

The raw image create params structure that is given to the tivxCreateRawImage function. More...

#include <tivx_ext_raw_image.h>

Data Fields

volatile vx_uint32 width
 The image width in pixels.
 
volatile vx_uint32 height
 The image height in lines (not including meta rows).
 
volatile vx_uint32 num_exposures
 The number of exposures contained in the sensor readout for a given timestamp. Max supported is TIVX_RAW_IMAGE_MAX_EXPOSURES.
 
volatile vx_bool line_interleaved
 A value of vx_true_e indicates that the exposures are line interleaved in a single contiguous buffer.
 
tivx_raw_image_format_t format [TIVX_RAW_IMAGE_MAX_EXPOSURES]
 Array of tivx_raw_image_format_t structures indicating the pixel packing and bit alignment format of each exposure. If line_interleaved == vx_false_e, then the number of valid structures in this array should be equal to the value of num_exposures. If line_interleaved == vx_true_e, then the format should be the same for each exposure in a single buffer, so the number of valid structures in this array should equal 1.
 
volatile vx_uint32 meta_height_before
 Number of lines of meta data at top of sensor readout (before pixel data) (uses the same width as original sensor readout width)
 
volatile vx_uint32 meta_height_after
 Number of lines of meta data at bottom of sensor readout (after pixel data) (uses the same width as original sensor readout width)
 

Detailed Description

The raw image create params structure that is given to the tivxCreateRawImage function.

Definition at line 117 of file tivx_ext_raw_image.h.


The documentation for this struct was generated from the following file: