TIOVX User Guide

The raw image format structure that is given to the tivxCreateRawImage function. More...

#include <tivx_ext_raw_image.h>

Data Fields

volatile vx_uint32 pixel_container
 Pixel Container, see tivx_raw_image_pixel_container_e.
 
volatile vx_uint32 msb
 Most significant bit in pixel container.
 

Detailed Description

The raw image format structure that is given to the tivxCreateRawImage function.

Definition at line 109 of file tivx_ext_raw_image.h.


The documentation for this struct was generated from the following file: