TIOVX User Guide

pyramid object descriptor as placed in shared memory More...

#include <tivx_obj_desc.h>

Data Fields

tivx_obj_desc_t base
 base object descriptor
 
volatile vx_uint32 num_levels
 number of pyramid levels
 
volatile vx_uint32 width
 width of the level0 image
 
volatile uint32_t height
 height of the level0 image
 
volatile vx_float32 scale
 Scaling factor between levels of the pyramid.
 
volatile vx_df_image format
 image format
 
volatile uint16_t obj_desc_id [TIVX_PYRAMID_MAX_LEVEL_OBJECTS]
 array of object descriptor ids for the image object
 

Detailed Description

pyramid object descriptor as placed in shared memory

Definition at line 617 of file tivx_obj_desc.h.


The documentation for this struct was generated from the following file: