TIOVX User Guide

threshold object descriptor as placed in shared memory More...

#include <tivx_obj_desc.h>

Data Fields

tivx_obj_desc_t base
 base object descriptor
 
volatile vx_enum type
 type of threshold
 
volatile int32_t value
 threshold value
 
volatile int32_t upper
 upper limit
 
volatile int32_t lower
 lower limit
 
volatile int32_t true_value
 threshold true value
 
volatile int32_t false_value
 threshold false value
 
volatile vx_enum data_type
 data type of the threshold
 

Detailed Description

threshold object descriptor as placed in shared memory

Definition at line 661 of file tivx_obj_desc.h.


The documentation for this struct was generated from the following file: