TIOVX User Guide

object array object descriptor as placed in shared memory More...

#include <tivx_obj_desc.h>

Data Fields

tivx_obj_desc_t base
 base object descriptor
 
volatile vx_enum item_type
 The item type of the lut.
 
volatile uint32_t num_items
 number of valid items in array
 
volatile uint16_t obj_desc_id [TIVX_OBJECT_ARRAY_MAX_ITEMS]
 array of descriptor ids of the objects
 

Detailed Description

object array object descriptor as placed in shared memory

Definition at line 784 of file tivx_obj_desc.h.


The documentation for this struct was generated from the following file: