TIOVX User Guide

Scalar object descriptor as placed in shared memory. More...

#include <tivx_obj_desc.h>

Data Fields

tivx_obj_desc_t base
 base object descriptor
 
volatile uint32_t data_type
 The value contained in the reference for a scalar type.
 
volatile uint32_t rsv
 Reserved field to make below union on 64b aligned boundary.
 
volatile vx_char chr
 A character.
 
volatile vx_int8 s08
 Signed 8 bit.
 
volatile vx_uint8 u08
 Unsigned 8 bit.
 
volatile vx_int16 s16
 Signed 16 bit.
 
volatile vx_uint16 u16
 Unsigned 16 bit.
 
volatile vx_int32 s32
 Signed 32 bit.
 
volatile vx_uint32 u32
 Unsigned 32 bit.
 
volatile vx_int64 s64
 Signed 64 bit.
 
volatile vx_uint64 u64
 Unsigned 64 bit.
 
volatile vx_float32 f32
 32 bit float
 
volatile vx_float64 f64
 64 bit float
 
volatile vx_df_image fcc
 32 bit image format code
 
volatile vx_enum enm
 Signed 32 bit.
 
volatile vx_size size
 Architecture depth unsigned value.
 
volatile vx_bool boolean
 Boolean Values.
 

Detailed Description

Scalar object descriptor as placed in shared memory.

Definition at line 802 of file tivx_obj_desc.h.


The documentation for this struct was generated from the following file: