TIOVX User Guide

array object descriptor as placed in shared memory More...

#include <tivx_obj_desc.h>

Data Fields

tivx_obj_desc_t base
 base object descriptor
 
tivx_shared_mem_ptr_t mem_ptr
 array memory address
 
volatile vx_enum item_type
 The item type of the array.
 
volatile uint32_t item_size
 Size of the array item.
 
volatile uint32_t num_items
 number of valid items in array
 
volatile uint32_t capacity
 Max size of the array.
 
volatile uint32_t mem_size
 size of buffer pointed to by mem_ptr
 

Detailed Description

array object descriptor as placed in shared memory

Definition at line 710 of file tivx_obj_desc.h.


The documentation for this struct was generated from the following file: