TIOVX User Guide

Remap object descriptor as placed in shared memory. More...

#include <tivx_obj_desc.h>

Data Fields

tivx_obj_desc_t base
 base object descriptor
 
tivx_shared_mem_ptr_t mem_ptr
 buffer address
 
volatile uint32_t src_width
 The source width.
 
volatile uint32_t src_height
 The source height.
 
volatile uint32_t dst_width
 The destination width.
 
volatile uint32_t dst_height
 The destination height.
 
volatile uint32_t mem_size
 size of buffer pointed to by mem_ptr
 

Detailed Description

Remap object descriptor as placed in shared memory.

Definition at line 544 of file tivx_obj_desc.h.


The documentation for this struct was generated from the following file: