8.7.8.128. OnReset()ΒΆ

GEL callback function called after the target processor has been reset.

Syntax

OnReset( intnErrorCode );

Parameters

nErrorCode: 0 (zero) indicates success.

Description

If defined in a loaded GEL file, OnReset() is called after the target processor has been reset.

Example

OnReset(int nErrorCode)
{
    if (nErrorCode)
    {
        GEL_TextOut("An error occurred while resetting. -%d-\n",,,,,nErrorCode);
    }
    else
    {
        GEL_TextOut("Reset was successful. -%d-\n",,,,, nErrorCode);
    }
}