8.7.8.3. GEL_AdvancedReset()ΒΆ

Resets processor.

Syntax

GEL_AdvancedReset( "reset_name", [synchronous = 1] );

Parameters

reset_name: specifies the name of the reset

synchronous (optional): is an optional integer parameter (defaulted to 1) where 1 means wait for the reset to be issued before returning to GEL and 0 means queue up the reset and return to GEL immediately.

Description

This GEL function issues any possible reset other than the default reset for the connected hardware device. Since some advanced resets don't indicate when the reset is complete, there is no way for this function to wait for the reset to complete, only to wait for the reset to be issued. However, for most advanced resets, this is the same thing.

Synchronous

Synchronous from GEL: Yes unless synchronous is set to 0

Completely synchronous: Yes unless synchronous is set to 0

Related Topics

GEL_Reset

GEL_Restart

GEL_Run

GEL_Halt

OnPreReset

OnReset