8.7.8.81. GEL_SetClockEventΒΆ
Configures the profile clock to profile an event.
Syntax
GEL_SetClockEvent( "event" );
Parameters
event: The name of the event for which the profile clock is to be configured. Note that these names vary by target.
Description
Configures the profile clock to profile the specified event. The clock count will be reset to zero. If there is no such event, this will throw an error and have no effect.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Example
GEL_SetClockEvent( "clock event name" );
Related Topics