8.7.8.17. GEL_EnableFileOutput()ΒΆ
Enables writing GEL Text output to a file
Syntax
GEL_EnableFileOutput( "filePath", [appendToEnd], [teeToConsole] );
Parameters
filePath: is the path of the file to which output should be written.
appendToEnd (optional): indicates whether to append to or overwrite a file. 0 - file content should be overwritten. 1 - append content. The default behaviour is to append.
teeToConsole (optional): indicates whether to send the output to the console as well. 0 - do not send the output. 1 - do send the output. The default behaviour is to send the output to the console.
Description
Enables writing GEL Text output generated by calls such as GEL_TextOut to a file specified by the filePath without affecting any other behaviour
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Example
GEL_EnableFileOutput("c:\\gel_out\\gel_log.txt");
GEL_EnableFileOutput("c:\\gel_out\\gel_log.txt" , 1);
GEL_EnableFileOutput("c:\\gel_out\\gel_log.txt", 0, 1);
Related Topics