8.7.8.57. GEL_MemoryLoadData()ΒΆ
Loads a block of memory from a file.
Syntax
GEL_MemoryLoadData( startAddress, page, length, "fileName" );
Parameters
startAddress: is the first address in the block.
page: identifies the type of memory to fill: 0 (Program memory), 1 (Data memory) or 2 (I/O space)
For processors that do not have more than one type of memory, use 0 for this Parameters. For simulated targets, the I/O space Parameters is not supported.
length: defines the number of values to load from the file
fileName: name of the file to load data from. The fileName must be enclosed in quotation marks.
Description
GEL_MemoryLoadData() is an extension to GEL_MemoryLoad() and supports loading data in additional formats to target memory from a specified file.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Example
GEL_MemoryLoadData( 0x100, 0 , 0x100, "c:\\mydir\\myfile.dat" );
Related Topics