8.7.8.121. OnFileLoaded()ΒΆ

GEL callback function called after a program is loaded.

Syntax

OnFileLoaded( intnErrorCode, intbSymbolsOnly );

Parameters

nErrorCode: 0 (zero) indicates success.

bSymbolsOnly: Boolean indicates if only symbols were loaded.

Description

If defined in a loaded GEL file, OnFileLoaded() is called after a program is loaded.

Example

OnFileLoaded(int nErrorCode, int bSymbolsOnly)
{
    if (nErrorCode)
    {
        GEL_TextOut("An error occurred while loading a file. -%d-\n",,,,,ErrorCode);
    }
    else
    {
        GEL_TextOut("File was loaded successfully. -%d-\n",,,,, nErrorCode);
    }
    if (bSymbolsOnly)
    {
        GEL_TextOut("Only symbols were loaded.\n");
    }
    else
    {
        GEL_TextOut("Full load.\n");
    }
}