8.7.8.83. GEL_SetSemihostingMainArgsΒΆ

Set the arguments that must be forwarded to the target program's main function in response to a SYS_GET_CMDLINE semihosting call.

Syntax

GEL_SetSemihostingMainArgs( args );

Parameters

args: String of arguments to be passed

Description

This function should be called to set the desired behaviour prior to calling GEL_Load to start a program load

Synchronous

Synchronous from GEL: Yes

Completely synchronous: No

Example

/* will pass an array of size 5 containing [arg1,arg2,arg3,arg4,arg5] */
GEL_SetSemihostingMainArgs("arg1 arg2 arg3 arg4 arg5")
/* will pass an array of size 4 containing [arg1, arg2 with space, arg3, arg4] */
GEL_SetSemihostingMainArgs("arg1 \"arg2 with space\" arg3 arg4")

Related Topics

GEL_Load