8.7.8.66. GEL_ProbePtDisableΒΆ

Disables a breakpoint at the specified address.

Syntax

GEL_ProbePtDisable( address );

Parameters

address: specifies the location of the breakpoint.

Description

The breakpoint at the specified address is disabled. If the breakpoint does not exist or is already disabled, no action is taken.

Synchronous

Synchronous from GEL: Yes

Completely synchronous: No

Example

GEL_ProbePtDisable(0x2000);
GEL_ProbePtDisable(main + 100);

Related Topics

GEL_ProbePtAdd

GEL_ProbePtDel